Click here to return to the Hardware Setup page
The AD243x high power evaluation boards used in the demos are explained in the following subsections.
Figure 1 shows a EVAL-AD2435WA3LZ board which can be used as a high power A2B main or a local powered A2B sub node. The board has following peripherals
Figure 1: EVAL-AD2435WA3LZ board
Figure 2 shows EVAL-AD2435WJ3LZ board which can be used as a high power bus powered A2B sub node. The board has following peripherals
Figure 2: EVAL-AD2435WJ3LZ board
To run the sample demo, the following setup connections are to be made.
A2B Evaluation boards shall be connected in the following order
Figure 3: A2B Eval board connections: High Power
For Aardvark, download and install the “USB Drivers – Windows” from Total Phase website.
Audio In/out