This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:a2bv2:quickstartguide:appendix-d [25 Nov 2022 06:28] – Gireesha Nirvanaiah | resources:tools-software:a2bv2:quickstartguide:appendix-d [25 Nov 2022 07:15] – Gireesha Nirvanaiah | ||
---|---|---|---|
Line 6: | Line 6: | ||
* To provide BCLK and Frame Sync to A2B transceiver, | * To provide BCLK and Frame Sync to A2B transceiver, | ||
* Under “DAI0 Pin Buffer” following changes need to be made. | * Under “DAI0 Pin Buffer” following changes need to be made. | ||
- | * **DAI0_PB03_I** which is routed to PCG0_CRS_CLKC_O by default should be routed removed and **PCG0_CLKA_O should be added**. Final configuration is shown in Figure 83. | + | * **DAI0_PB03_I** which is routed to PCG0_CRS_CLKC_O by default should be routed removed and **PCG0_CLKA_O should be added**. Final configuration is shown in Figure 83. {{ : |
- | * **DAI0_PB04_I** which is routed to PCG0_CRS_FSC_O by default should be routed removed and **PCG0_FSA_O should be added**. Final configuration is shown in | + | * **DAI0_PB04_I** which is routed to PCG0_CRS_FSC_O by default should be routed removed and **PCG0_FSA_O should be added**. Final configuration is shown in {{ : |
- | * In the file “C: | + | * In the file “C: |
* Once these changes are made, build the project and copy the generated .dxe file to <<A2B plugin for SigmaStudio+ installation path>> | * Once these changes are made, build the project and copy the generated .dxe file to <<A2B plugin for SigmaStudio+ installation path>> | ||
* Use “LDR_gen.bat” script available in <<A2B plugin for SigmaStudio+ installation path>> | * Use “LDR_gen.bat” script available in <<A2B plugin for SigmaStudio+ installation path>> |