This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:a2bv2:quickstartguide:appendix-a [09 Oct 2023 12:23] – agnes monica | resources:tools-software:a2bv2:quickstartguide:appendix-a [20 Dec 2023 12:19] (current) – [Network Properties] Gireesha Nirvanaiah | ||
---|---|---|---|
Line 20: | Line 20: | ||
* EVAL- AD2438WD1BZ: | * EVAL- AD2438WD1BZ: | ||
* EVAL- AD2437A1NZ: This can be used as both a main and a sub node | * EVAL- AD2437A1NZ: This can be used as both a main and a sub node | ||
- | * EVAL-AD2437B1NZ: | + | * EVAL- AD2437B1NZ: This is a sub node only platform. |
+ | * EVAL- AD2437A1MZ: This can be used as both a main and a sub node. | ||
+ | * EVAL- AD2437B1MZ: This is a sub node only platform. | ||
- **A2BBusAnalyzer** | - **A2BBusAnalyzer** | ||
- **AD242x:** This can be used for Main/Sub Node Emulation or Bus Monitoring of 242x transceiver variants on the A2B Bus Analyzer Hardware | - **AD242x:** This can be used for Main/Sub Node Emulation or Bus Monitoring of 242x transceiver variants on the A2B Bus Analyzer Hardware | ||
Line 33: | Line 35: | ||
* Generic device: A device that takes an xml file as input for programming via I2C. | * Generic device: A device that takes an xml file as input for programming via I2C. | ||
* Non-Programmable generic device: A device that is used for representing not programmable peripherals in A2B system (e.g. Microphone). | * Non-Programmable generic device: A device that is used for representing not programmable peripherals in A2B system (e.g. Microphone). | ||
- | These devices are available as part of the toolbox once inside the platform view/canvas as shown in **Error! Reference source not found..** The platform canvas can be opened by double clicking on the platform in the system view or by clicking the “Canvas” option under the platform in the Project window. | + | These devices are available as part of the toolbox once inside the platform view/canvas as shown in below, the platform canvas can be opened by double clicking on the platform in the system view or by clicking the “Canvas” option under the platform in the Project window. |
==== Transceiver settings (General View, Register View, Stream View and Crossbar View) ==== | ==== Transceiver settings (General View, Register View, Stream View and Crossbar View) ==== | ||
Line 70: | Line 72: | ||
**Modified: | **Modified: | ||
- | **Optimized: | + | **Optimized: |
**Advanced: | **Advanced: | ||
Line 77: | Line 79: | ||
The Line Fault settings allow user to enable fault diagnostic feature of the software. With this any line fault encountered in the system is handled and reported to the user. | The Line Fault settings allow user to enable fault diagnostic feature of the software. With this any line fault encountered in the system is handled and reported to the user. | ||
+ | |||
+ | **Override Bus Self Discovery: | ||
**Enable Line Fault Diagnostics: | **Enable Line Fault Diagnostics: |