This is an old revision of the document!
Click here to return to the QSG homepage
The A2B Plugin for SigmaStudio+ gives the following default platforms for the user:
Refer Hardware configuration Tab for more details.
Figure 56: A2B platforms in toolbox
In addition to these, the plugin also provides a range of transceivers and generic peripheral devices as follows:
These devices are available as part of the toolbox once inside the platform view/canvas as shown in Error! Reference source not found.. The platform canvas can be opened by double clicking on the platform in the system view or by clicking the “Canvas” option under the platform in the Project window.
The transceivers and peripheral settings window can be opened by double clicking on the transceiver/peripheral in the platform view. Additionally, it can also be opened by clicking on the “Settings” option under the transceiver/peripheral in the project window.
Figure 57: A2B transceivers and generic devices
Figure 58 : General View
Figure 59 : Register View
Figure 60: Node Level Stream View
The Network Properties tab, as shown in Figure 61, offers configurable options for the target processor software. With these settings one can select the node discovery and initialization method to be used and the clock source for the A2B network.
Figure 61: Network Properties Tab
The four possible discovery methods are
Simple: All sub nodes are discovered sequentially from sub 0 to the last available sub node in the system. Once all the sub nodes are discovered, they are initialized for synchronous data exchange.
Modified: All sub nodes are discovered and immediately initialized (for synchronous data exchange) sequentially from sub 0 to the last available sub node in the system.
Optimized: Even before a node is initialized the host tries to discover the next node. The time for the next node to be discovered is used to initialize the current node. Synchronous data can start only after all nodes are discovered and initialized (not supported for AD2430 AND AD2438).
Advanced: Even before a node is initialized the host tries to discover the next node. The time for the next node to be discovered is used to initialize the current node. Synchronous data exchange can start as soon as a main and sub node 0 is initialized (not supported for AD243x main).
Discovery Start Delay (ms): Delay (in milliseconds) to wait after a software reset and before discovery start.
The Line Fault settings allow user to enable fault diagnostic feature of the software. With this any line fault encountered in the system is handled and reported to the user.
Enable Line Fault Diagnostics: Enables line fault diagnostic feature of software. When set, SigmaStudio+ will continuously monitor the network for faults at 1 second interval. Detected faults will be handled and notified.
Rediscovery upon faults: If checked, automatic network rediscovery will be performed upon detecting post-discovery faults.
Stack Debug Settings: This feature allows the user to analyse/ understand the system by using the information logged during stack execution. Information can be either through TRACE or sequence chart or both.