The procedure to use optoA2B with A2B Bus Analyzer is as follows:
This section will guide the user to configure an OptoA2B branch network using ADI’s A2B Bus Analyzer as main node in the following configuration:
A2B Analyzer ←→ Opto A2B Sub←→ Opto A2B Main ←→ A2B Sub node DUT
SI No. | Software Component | Version | Comments |
---|---|---|---|
1. | SigmaStudio+ | 2.1.0 or later | SS+ Guide |
2. | A2B | 1.3.1 or later | User Guide |
3. | A2B Bus Analyzer | 3.4 or later | Quick Start Guide |
A2B Analyzer ←→ Opto A2B Sub ←→ Opto A2B Main ←→ A2B Sub node DUT
Project file: <Installation Path>\ADI_A2B-SSPlus_Software-Relx.y.z\Schematics\A2BBusAnalyzer\adi_a2bbusanalyzer_243xStdPwrMain_242xOptoA2B.ssproj
Sl. No | Name of Board | Type of Board/ Node | Quantity |
---|---|---|---|
1 | A2B Bus Analyzer kit | Emulated as Main node | 1 |
2 | Twisted Pair A2B Cable | DuraClik connector on one end to Analyzer and Rosenberger HSD connector on one end to OptoA2B Main | 1 |
3 | 12V Power Supply | - | 2 |
4 | USB cable from PC to A2B Bus Analyzer | - | 1 |
5 | Audio source (non-grounded) | e.g., PC/Mobile phone | 1 |
6 | Aux Cable | - | 1 |
7 | Audio Sink Devices | 3.5mm Jack Headphones | 1 |
8 | AD2428WD1BZ (for emulating optoA2B only) | Primary chain-sub, Branch Main, Branch Sub - NOT required when actual optoA2B is available | 3 |
OptoA2B main and DUT are present inside the EMC chamber while A2B Bus Analyzer and optoA2B sub are outside the chamber.
A2B Analyzer to be kept in Standard power Emulator mode.
Procedure to run a Branch Network (Opto A2B) from ADI A2B Analyzer:
Opto A2B Sub to Opto A2B main (in the current example AD2428WD1BZ is used for Opto Sub and Opto main)
Jumper | Opto Sub to Opto Main |
---|---|
JP5 (BCLK) | 3 → 3 |
JP6 (SYNC) | 3 → 3 |
DRX0 - DTX0 | 3(JP7) → 2(JP10) |
DRX1 - DTX1 | 2(JP8) → 3(JP9) |
DTX0 - DRX0 | 2(JP10) → 3(JP7) |
DTX1 - DRX1 | 3(JP9) → 2(JP8) |
P1(SCL) | 1 → 1 |
P1(SDA) | 3 → 3 |
P1(GND) | 10 → 10 |
A2B Sub node DUT (in the current example – AD2428WD1BZ is used as Sub node DUT)
Jumper | LPS | Comments |
---|---|---|
JP1 (A2B power) | Install | - |
JP2 | Uninstall | Install when phantom power or hybrid power support is required |
JP3 | Uninstall | Install when phantom power or hybrid power support is required |
JP4 (BOOT) | Install | Self-Boot option disabled. |
JP5 (BCLK) | 1-3 | AD2428_BCLK → ADAU1961_BCLK |
JP6 (SYNC) | 1-3 | AD2428_SYNC → ADAU1961_LRCLK |
JP7 (DRX0) | 1-3 | ADAU1961_ADC → AD2428_DRX0 |
JP8 (DRX1) | Uninstall | - |
JP9 (DTX1) | Uninstall | - |
JP10 (DTX0) | 2-3 | AD2428_DTX0 → ADAU1961_DAC |
JP11 (ADMP621 CLK) | Uninstall | - |
JP12 (NTC) | Install | - |
JP13 (A2B_REG) | Uninstall | - |
JP14 (VOLTAGE) | Uninstall | Install/ Uninstall depending on VIN requirement. Installed → VIN = 7V, Uninstalled → VIN = 8V |
JP19 (1961 BCLK) | 2-3 | ADAU1761 MCLK from AD2428_BCLK |