This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:technical-guides:surge [05 Jul 2022 14:11] – s valerie hamilton | resources:technical-guides:surge [09 Sep 2022 12:07] (current) – s valerie hamilton | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====Surge Test Results==== | + | ====AD74115H |
The surge immunity test indicates the capability of the device or equipment to survive surges caused by events such as lightning strikes or industrial power surges caused by switching heavy loads or short-circuit fault conditions. | The surge immunity test indicates the capability of the device or equipment to survive surges caused by events such as lightning strikes or industrial power surges caused by switching heavy loads or short-circuit fault conditions. | ||
- | Per the IEC 61000-4-5 standard for industrial environments, | + | Per the IEC 61000-4-5 standard for industrial environments, |
- | The CDNs do not influence the specified functional conditions of the EUT. The interconnection line between the EUT and the CDN is 2 m in length or shorter | + | The CDNs (coupling decoupling network) |
===Table 1 IEC 61000-4-5 Surge Test Levels=== | ===Table 1 IEC 61000-4-5 Surge Test Levels=== | ||
Line 24: | Line 24: | ||
\\ | \\ | ||
===Hardware Configuration=== | ===Hardware Configuration=== | ||
- | The use cases tested during surge testing were voltage output (and by default | + | The use cases tested during surge testing were voltage output (and voltage input by reconfiguring the ADC input nodes), internal digital output sourcing and sinking. The external sense pins SENSE_EXT1 and SENSE_EXT2 were also subject to testing. The reasoning for these particular use cases were to ensure the integrity of the I/O and sense screw terminals along with the internal fets used for the internal digital output use case. The surge was coupled to each screw terminal one at a time with respect to IO_N (AGND). Unshielded cable was used for all use cases. |
\\ | \\ | ||
- | For the voltage output use case, 6 V was configured as the output into a 100 kΩ load connected between IO_P and IO_N. The measurement (voltage input) was configured as IO_P to IO_N. The SENSE_EXT1 and SENSE_EXT2 nodes were selected as diagnostic nodes and configured as inputs to the ADC also. | + | For the voltage output use case, 6 V was configured as the output into a 100 kΩ load connected between IO_P and IO_N. The measurement (voltage input) was configured as IO_P to IO_N in the range 0 V to 12 V. The SENSE_EXT1 and SENSE_EXT2 nodes were selected as diagnostic nodes and configured as inputs to the ADC in the range 0 V to 12 V. Two AA batteries connected in series were used as a 3.1 V input to each of the SENSE_EXTx pins. |
For internal digital output a 1 kΩ load resistor was connected between IO_P and IO_N. The measurement was configured for the internal diagnostic of current flowing through the internal RSET. | For internal digital output a 1 kΩ load resistor was connected between IO_P and IO_N. The measurement was configured for the internal diagnostic of current flowing through the internal RSET. | ||
Line 53: | Line 53: | ||
===Performance Summary=== | ===Performance Summary=== | ||
- | Table 2 gives a summary of the surge test results. For the digital output use cases a deviation is not recorded as the accuracy is dependent on the load. The test verified that the digital output did not turn off unexpectedly. | + | Table 2 gives a summary of the surge test results. For the digital output use cases a deviation is not recorded as the accuracy is dependent on the load. The test verified that the digital output did not turn off unexpectedly. |
\\ | \\ | ||
===Table 2 Surge Results=== | ===Table 2 Surge Results=== | ||
- | ^ Test Level ^ Use Case ^ Pre Test Average | + | ^ Test Level ^ Use Case ^ Pre Test Measurement |
- | | 1 kV | Voltage Output | + | | 1 kV | Voltage Output |
- | | ::: | SENSE EXT1 | + | | ::: | SENSE EXT1 |
- | | ::: | SENSE EXT2 | + | | ::: | SENSE EXT2 |
| ::: | Digital Output Internal Source | | ::: | Digital Output Internal Source | ||
| ::: | Digital Output Internal Sink | 22.49 mA | 22.49 mA | N/A | Class B | | | ::: | Digital Output Internal Sink | 22.49 mA | 22.49 mA | N/A | Class B | | ||
- | | − 1 kV | Voltage Output | + | | − 1 kV | Voltage Output |
- | | ::: | SENSE EXT1 | + | | ::: | SENSE EXT1 |
- | | ::: | SENSE EXT2 | + | | ::: | SENSE EXT2 |
| ::: | Digital Output Internal Source | | ::: | Digital Output Internal Source | ||
| ::: | Digital Output Internal Sink | 22.49 mA | 22.49 mA | N/A | Class B | | | ::: | Digital Output Internal Sink | 22.49 mA | 22.49 mA | N/A | Class B | | ||
+ | \\ | ||
+ | [[resources: |