This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:technical-guides:surge [01 Jul 2022 16:19] – s valerie hamilton | resources:technical-guides:surge [09 Sep 2022 12:07] (current) – s valerie hamilton | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====Surge Test Results==== | + | ====AD74115H |
The surge immunity test indicates the capability of the device or equipment to survive surges caused by events such as lightning strikes or industrial power surges caused by switching heavy loads or short-circuit fault conditions. | The surge immunity test indicates the capability of the device or equipment to survive surges caused by events such as lightning strikes or industrial power surges caused by switching heavy loads or short-circuit fault conditions. | ||
- | Per the IEC 61000-4-5 standard for industrial environments, | + | Per the IEC 61000-4-5 standard for industrial environments, |
- | The CDNs do not influence the specified functional conditions of the EUT. The interconnection line between the EUT and the CDN is 2 m in length or shorter | + | The CDNs (coupling decoupling network) |
===Table 1 IEC 61000-4-5 Surge Test Levels=== | ===Table 1 IEC 61000-4-5 Surge Test Levels=== | ||
Line 24: | Line 24: | ||
\\ | \\ | ||
===Hardware Configuration=== | ===Hardware Configuration=== | ||
- | The use cases tested during surge testing were voltage output (and by default | + | The use cases tested during surge testing were voltage output (and voltage input by reconfiguring the ADC input nodes), internal digital output sourcing and sinking. The external sense pins SENSE_EXT1 and SENSE_EXT2 were also subject to testing. The reasoning for these particular use cases were to ensure the integrity of the I/O and sense screw terminals along with the internal fets used for the internal |
+ | \\ | ||
+ | |||
+ | |||
+ | For the voltage output use case, 6 V was configured as the output into a 100 kΩ load connected between IO_P and IO_N. The measurement (voltage input) was configured as IO_P to IO_N in the range 0 V to 12 V. The SENSE_EXT1 and SENSE_EXT2 nodes were selected as diagnostic nodes and configured as inputs to the ADC in the range 0 V to 12 V. Two AA batteries connected in series were used as a 3.1 V input to each of the SENSE_EXTx pins. | ||
+ | |||
+ | For internal digital output a 1 kΩ load resistor was connected between IO_P and IO_N. The measurement was configured for the internal diagnostic of current flowing through the internal RSET. | ||
===Software Configuration=== | ===Software Configuration=== | ||
- | The software was written in python to facilitate interaction | + | The software |
Pre test configuration | Pre test configuration | ||
*Reset DUT | *Reset DUT | ||
Line 40: | Line 47: | ||
*Read and store alert status register | *Read and store alert status register | ||
*Clear alert status register | *Clear alert status register | ||
- | *Read ADC code | + | *Read ADC data |
- | *Read DMM measurement | + | |
*Save data to file | *Save data to file | ||
- | *Repeat 1000 times | ||
\\ | \\ | ||
+ | |||
===Performance Summary=== | ===Performance Summary=== | ||
- | Table 2 gives a summary of the immunity | + | Table 2 gives a summary of the surge test results. |
+ | \\ | ||
- | ===Table 2=== | + | ===Table 2 Surge Results=== |
- | ^Test ^Use Case ^Standard | + | ^ Test Level |
- | |Surge| Voltage Output| | + | | 1 kV |
- | |:::| Voltage Input| :::| :::|:::|:::| | + | | ::: | SENSE EXT1 | |
- | |:::| Digital Output Internal Sink and Source| :::| ::: | + | | |
+ | | | ||
+ | | ::: | Digital Output Internal Sink | 22.49 mA | 22.49 mA | N/A | Class B | | ||
+ | | − 1 kV | Voltage Output | ||
+ | | | ||
+ | | | ||
+ | | | ||
+ | | | ||
\\ | \\ | ||
+ | [[resources: |