This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:technical-guides:surge [12 Aug 2022 17:42] – s valerie hamilton | resources:technical-guides:surge [09 Sep 2022 12:07] (current) – s valerie hamilton | ||
---|---|---|---|
Line 2: | Line 2: | ||
The surge immunity test indicates the capability of the device or equipment to survive surges caused by events such as lightning strikes or industrial power surges caused by switching heavy loads or short-circuit fault conditions. | The surge immunity test indicates the capability of the device or equipment to survive surges caused by events such as lightning strikes or industrial power surges caused by switching heavy loads or short-circuit fault conditions. | ||
- | Per the IEC 61000-4-5 standard for industrial environments, | + | Per the IEC 61000-4-5 standard for industrial environments, |
- | The CDNs do not influence the specified functional conditions of the EUT. The interconnection line between the EUT and the CDN is 2 m in length or shorter | + | The CDNs (coupling decoupling network) |
===Table 1 IEC 61000-4-5 Surge Test Levels=== | ===Table 1 IEC 61000-4-5 Surge Test Levels=== | ||
Line 24: | Line 24: | ||
\\ | \\ | ||
===Hardware Configuration=== | ===Hardware Configuration=== | ||
- | The use cases tested during surge testing were voltage output (and by default | + | The use cases tested during surge testing were voltage output (and voltage input by reconfiguring the ADC input nodes), internal digital output sourcing and sinking. The external sense pins SENSE_EXT1 and SENSE_EXT2 were also subject to testing. The reasoning for these particular use cases were to ensure the integrity of the I/O and sense screw terminals along with the internal fets used for the internal digital output use case. The surge was coupled to each screw terminal one at a time with respect to IO_N (AGND). Unshielded cable was used for all use cases. |
\\ | \\ | ||