This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:technical-guides:network-application-user-guide [23 Mar 2023 13:13] – [Structure of the network-application:] Christopher Stelmar | resources:technical-guides:network-application-user-guide [03 Apr 2023 16:34] (current) – old revision restored (22 Mar 2023 21:57) Christopher Stelmar | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Network-app Documentation ====== | ====== Network-app Documentation ====== | ||
+ | |||
+ | For creating a network application, | ||
+ | |||
+ | This document works for those who are attempting to create a network application from scratch with IE stacks. This has no use without appropriate hardware and software. | ||
===== Structure of the network-application: | ===== Structure of the network-application: | ||
Line 5: | Line 9: | ||
There are two types of assets, namely Interface Assets and Functional Assets. | There are two types of assets, namely Interface Assets and Functional Assets. | ||
- | ===== Interface Assets: | + | Interface Assets: |
These are the assets that provide the network application with an interface to functionality that is part of the IO application. | These are the assets that provide the network application with an interface to functionality that is part of the IO application. | ||
For example, the asset network-os-srv asset extracts the freertos functionality by requesting the APIs from the freertos-ospl-srv asset that is part of the io-app workspace. | For example, the asset network-os-srv asset extracts the freertos functionality by requesting the APIs from the freertos-ospl-srv asset that is part of the io-app workspace. |