Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:technical-guides:best_engineering_practices_when_using_adxl_accelerometers [29 Mar 2021 17:42] Pablo del Corroresources:technical-guides:best_engineering_practices_when_using_adxl_accelerometers [15 Mar 2022 14:41] (current) Pablo del Corro
Line 9: Line 9:
 The first and most important advise we would like to offer when using our ADXL portfolio is to **carefully read the product datasheet**, this can save you precious time.  The first and most important advise we would like to offer when using our ADXL portfolio is to **carefully read the product datasheet**, this can save you precious time. 
  
-===== Terminology =====+===== Common terminology in ADXL's datasheet specifications =====
  
 === Full-Scale Range (FSR) ===  === Full-Scale Range (FSR) === 
Line 17: Line 17:
 Device nonlinearity is the maximum deviation of any sensor data point from the least squares linear fit of the acceleration data set at an equivalent input acceleration level. The acceleration data set can encompass any range of applied acceleration, up to the complete FSR. Nonlinearity is defined mathematically as Device nonlinearity is the maximum deviation of any sensor data point from the least squares linear fit of the acceleration data set at an equivalent input acceleration level. The acceleration data set can encompass any range of applied acceleration, up to the complete FSR. Nonlinearity is defined mathematically as
  
-{{ :resources:technical-guides:nonlinearity.png?nolink&300 |}}+{{ :resources:technical-guides:nonlinearity.png?nolink&250 |}}
  
 where: where:
Line 29: Line 29:
 Cross axis sensitivity is the measured output of the device in response to input stimuli orthogonal to the intended sense axis. It is measured as a percentage of the applied acceleration, as follows: Cross axis sensitivity is the measured output of the device in response to input stimuli orthogonal to the intended sense axis. It is measured as a percentage of the applied acceleration, as follows:
  
-{{ :resources:technical-guides:crossaxissen.png?nolink&300 |}}+{{ :resources:technical-guides:crossaxissen.png?nolink&250 |}}
  
 where: where:
Line 40: Line 40:
 === Resonant Frequency (fo) === === Resonant Frequency (fo) ===
 fo is the natural frequency at which the MEMS element has  a higher gain when subjected to acceleration events. Input acceleration at this resonant frequency causes the sensor to displace by an amount equal to the applied acceleration multiplied by the quality factor (Q). fo is the natural frequency at which the MEMS element has  a higher gain when subjected to acceleration events. Input acceleration at this resonant frequency causes the sensor to displace by an amount equal to the applied acceleration multiplied by the quality factor (Q).
-Some parts, for example the ADXL317, use different sensor types for the horizontal (x- and y-axes) and the vertical (z-axis) sensing axes. Therefore, the resonant frequency responses of these sensors are not the same.+Some parts use different sensor types for the horizontal (x- and y-axes) and the vertical (z-axis) sensing axes. Therefore, the resonant frequency responses of these sensors are not the same.
  
 === Quality Factor === === Quality Factor ===
 The quality factor is a scalar factor that governs the increase or decrease in amplitude of an acceleration signal applied at the resonant frequency of a MEMS element. The quality factor is a scalar factor that governs the increase or decrease in amplitude of an acceleration signal applied at the resonant frequency of a MEMS element.
  
 +=== Sensitivity ===
 +Sensitivity is the slope of the line of best fit for the acceleration transfer function, as measured across the output FSR. The sensitivity defines the change in output (LSB) per unit change of input (g). The inverse, scale factor, is in units of g/LSB.
  
-===== Power supply considerations =====  +{{ :resources:technical-guides:sensitivity.png?nolink&400 |}}
-It is important to respect the power supply limits and considerations described in the datasheet+
  
-<note tip>As a general ruleit is __highly recommended__ to always be started up the accelerometer from ground level (0 V).</note> +=== Measurement Resolution === 
 +Measurement resolution specifies the number of data bits in each acceleration data-word. For examplethe 14-bit measurement of the ADXL317 has 16,384 bits of resolution. For an FSR of ±16 g (32 g total), this resolution yields a sensitivity of 500 LSB/g and a scale factor of 2.0 mg/LSB. 
 + 
 +=== Zero g Bias Error === 
 +The zero g bias error (also called offset) is any static error term on the sensor output. Zero g bias error is measured as the deviation from 0 g with no externally applied acceleration (including gravity). 
 +To more accurately measure offset, take measurements at orientations of +1 g and –1 g and average the results. Each measurement must be taken over a sufficiently long time window to reduce the influence of external physical stimuli  
 +that may exist in the measurement system. 
 + 
 +{{ :resources:technical-guides:offset.png?nolink&400 |}}  
 + 
 +=== Initial Zero g Output Deviation === 
 +Initial zero g output deviation is the error level at ambient conditions, measured immediately after completion of device manufacture. The initial zero g output deviation value denotes the standard deviation of the measured offset values across a large population of devices. 
 + 
 +=== Cutoff (−3 dBFrequency === 
 +For applied ac acceleration, the cutoff (−3 dB) frequency is the frequency at which the input stimulus is attenuated in amplitude by 29.3% (1 − √2/2) at the output of the signal chain.  
 + 
 +===== Power supply considerations =====  
 +It is important to respect the power supply limits and considerations described in the datasheet. For example, for the ADXL34x devices, supply limits are specified from 2V to 3.6V, utilizing the sensor at lower voltages than 2V can result in improper operation, whereas applying higher voltages than 3.6V can permanently damage the device. 
  
 === Recommended VS and VDDIO power sequencing ===  === Recommended VS and VDDIO power sequencing === 
Line 59: Line 77:
 === Power Cycling ===  === Power Cycling === 
 It is common in ULP applications to power cycle the accelerometer to reduce power consumption. When using this technique, please remember that it is highly recommend to always start up the accelerometer from ground level (0 V) to ensure proper operation.  It is common in ULP applications to power cycle the accelerometer to reduce power consumption. When using this technique, please remember that it is highly recommend to always start up the accelerometer from ground level (0 V) to ensure proper operation. 
 +
 +<note tip>As a general rule, it is __highly recommended__ to always be started up the accelerometer from ground level (0 V).</note> 
 +
 If this is not possible, care must be taken regarding the following specifications: If this is not possible, care must be taken regarding the following specifications:
  
-  * __**VS supply start-up threshold**__: During start-up or power cycling, the VS and VDDIO supplies must always be started up from below 100 mVWhen the device is in operation, any time power is removed or falls below the accelerometer power supply lower range voltage, VS and VDDIO supplies must be discharged below 100 mV. **This specification is mandatory**. +  * __**V <wrap lo>RESET</wrap>**__: During start-up or power cycling, the VS and VDDIO supplies must always be started up from below V_RESET voltageAlso, when the device is in operation, any time power is removed or falls below the accelerometer power supply lower range voltage (VS_MIN), VS and VDDIO supplies must be discharged below V_RESET and powered back up for proper operation. **This specification is mandatory**. 
-  * __**Hold time**__: VS and VDDIO supplies must be held below 100 mV for at least 200 ms before re-powering the part. +  * __**Hold time**__: VS and VDDIO supplies must be held below V_RESET for at least the specified hold time before re-powering the part. 
-  * __**Rise time**__: For the worst case scenario (100mV Vs starts up and 200ms hold time) VS and VDDIO supplies rise time must be linear and within 250 μs to reach the supply lower range voltage. For example, for the ADXL372, the power supply lower range voltage is 1.6V, thus the voltage supply should raise from 0V to 1.6V within 250μs+  * __**Rise time**__: The supply voltage rise time is defined as the time from 0 V to 90% of VS. 
 + 
 +{{ :resources:technical-guides:por_graph_generic.png?400 |}}
  
-{{ :resources:technical-guides:adxl372_revc_por_graph.jpg?nolink&400 |}}+For example for the ADXL362 and ADXL37x devices, the power cycling requirements are 
 +  * __**V <wrap lo>RESET</wrap>**__equal or lower than 100 [mV]. 
 +  * __**Hold time**__: equal or grater than 200 [ms]. 
 +  * __**Rise time**__should be linear and with a slope equal or higher than 6 [V/ms]
  
-<note>Fully discharging the power supply to the ground level allows a much more relaxed rise time, ≤600 µs, from 0 to supply lower range voltage, for a 200 ms hold time.</note>+<note>Fully discharging the power supply to the ground level allows a much more relaxed rise time. For the example of ADXL362 and ADXL37x devicesthe rise time slope can be as low as 2.5 [V/ms], for a 200 [mshold time.</note>
      
 To enable supply discharge, it is recommended to power the device from a microcontroller general-purpose input/output (GPIO), connect a shutdown discharge switch to the supply, or use a voltage regulator with a shutdown discharge feature.  To enable supply discharge, it is recommended to power the device from a microcontroller general-purpose input/output (GPIO), connect a shutdown discharge switch to the supply, or use a voltage regulator with a shutdown discharge feature. 
resources/technical-guides/best_engineering_practices_when_using_adxl_accelerometers.1617032557.txt.gz · Last modified: 29 Mar 2021 17:42 by Pablo del Corro