This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:technical-guides:best_engineering_practices_when_using_adxl_accelerometers [12 Feb 2021 20:26] – Pablo del Corro | resources:technical-guides:best_engineering_practices_when_using_adxl_accelerometers [29 Mar 2021 17:30] – Pablo del Corro | ||
---|---|---|---|
Line 21: | Line 21: | ||
=== Power Cycling === | === Power Cycling === | ||
- | It is common in ULP applications to power cycle the accelerometer to reduce power consumption. When using this technique, please remember that it is highly recommend to always | + | It is common in ULP applications to power cycle the accelerometer to reduce power consumption. When using this technique, please remember that it is highly recommend to always |
If this is not possible, care must be taken regarding the following specifications: | If this is not possible, care must be taken regarding the following specifications: | ||
- | * __**VS supply start-up threshold**__: | + | * __**VS supply start-up threshold**__: |
- | * __**Hold time**__: VS and VDDIO supplies must be held below 200 mV for at least 100 ms before re-powering the part. | + | * __**Hold time**__: VS and VDDIO supplies must be held below 100 mV for at least 200 ms before re-powering the part. |
- | * __**Rise time**__: For the worst case scenario, 200mV Vs starts up and 100ms hold time, VS and VDDIO supplies rise time must be linear and within | + | * __**Rise time**__: For the worst case scenario |
- | Hold time and rise time specifications can vary. For example, if hold time is much longer than 100ms, the rise time criteria might be relaxed. The user should carefully select the start-up specifications that suits their application. | + | {{ : |
- | < | + | < |
| | ||
To enable supply discharge, it is recommended to power the device from a microcontroller general-purpose input/ | To enable supply discharge, it is recommended to power the device from a microcontroller general-purpose input/ |