This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:quick-start:adin1110_linux_quick_start_guide [05 Dec 2022 06:47] – Alexandru Tachici | resources:quick-start:adin1110_linux_quick_start_guide [05 Dec 2022 06:55] – Alexandru Tachici | ||
---|---|---|---|
Line 24: | Line 24: | ||
ADIN1110 needs to operate in Generic SPI mode (see Datasheet) and with CRC protection enabled. In order to do this find S201 and set every switch to the following table: | ADIN1110 needs to operate in Generic SPI mode (see Datasheet) and with CRC protection enabled. In order to do this find S201 and set every switch to the following table: | ||
- | ^ SWTICH | + | ^ SWITCH |
| SPI_CFG0 | | SPI_CFG0 | ||
| SPI_CFG1 | | SPI_CFG1 | ||
Line 68: | Line 68: | ||
ADIN1110 needs to operate in Generic SPI mode (see Datasheet) and with CRC protection enabled. In order to do this find S201 and set every switch to the following table: | ADIN1110 needs to operate in Generic SPI mode (see Datasheet) and with CRC protection enabled. In order to do this find S201 and set every switch to the following table: | ||
- | ^ SWTICH | + | ^ SWITCH |
| SPI_CFG0 | | SPI_CFG0 | ||
| SPI_CFG1 | | SPI_CFG1 | ||
Line 75: | Line 75: | ||
| MS_SEL | | MS_SEL | ||
- | Make sure IMX8MM-BB is set to boot from the SD Card, for more details go to [[https:// | + | Make sure IMX8MM-BB is set to boot from the SD Card, for more details go to [[https:// |
Line 235: | Line 235: | ||
In order to do this find S1 and set every switch to the following table: | In order to do this find S1 and set every switch to the following table: | ||
- | ^ SWTICH | + | ^ SWITCH |
| SPI_CFG0 | | SPI_CFG0 | ||
| SPI_CFG1 | | SPI_CFG1 | ||
Line 241: | Line 241: | ||
| TX2V4_DIS | OFF | | | TX2V4_DIS | OFF | | ||
| MS_SEL | | MS_SEL | ||
- | |||
- | === Board settings === | ||
- | |||
- | ADIN1110 needs to operate in Generic SPI mode (see Datasheet) and with CRC protection disabled. You may enable the CRC but that needs a change in the DT also. | ||
- | See [[https:// | ||
- | |||
== Getting your Jetson Nano flashed with the SDK Manager == | == Getting your Jetson Nano flashed with the SDK Manager == | ||
Line 316: | Line 310: | ||
| kernel/ | | kernel/ | ||
| kernel/ | | kernel/ | ||
- | | kernel/ | + | | kernel/ |
| kernel/ | | kernel/ | ||
| kernel/ | | kernel/ |