This is an old revision of the document!
make
This is the complete compilation process. It is made up of three rules, that can be used separately:
make project
- creates the build
directory and the required directory structure
- uses SDK to create a project under the build
directory
make update
- updates the no-OS sources under the build
directory with files specified in src.mk
make build
- performs the build of files under the build
directory using gcc
make sdkbuild
- performs the build of files under the build
directory using SDK
When modifications are performed, the following three commands trigger the necessary clean actions:
make clean
- deletes the artifacts generated during build
make reset
- deletes the build
directory (this results in a fresh setup for starting the complete compilation process)
make sdkclean
- cleans the artifacts (.o, .elf, .hex, etc.) created by the build command using the SDK
make run
- downloads and runs the executable on the target board
make debug
- downloads the executable on the target board and opens a command-line gdb
instance to
debug it (only on some platforms)