This shows you the differences between two versions of the page.
— | resources:no-os:iio [07 Jun 2022 15:06] (current) – initial version - wip Dragos Bogdan | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== no-OS IIO ====== | ||
+ | To get registered with the no-OS IIO framework, each device should export a populated **struct iio_device** - what data can be accessed by an IIO client is defined here: | ||
+ | |||
+ | < | ||
+ | struct iio_device { | ||
+ | struct no_os_irq_ctrl_desc *irq_desc; | ||
+ | uint16_t num_ch; | ||
+ | struct iio_channel *channels; | ||
+ | struct iio_context_attribute *context_attributes; | ||
+ | struct iio_attribute *attributes; | ||
+ | struct iio_attribute *debug_attributes; | ||
+ | struct iio_attribute *buffer_attributes; | ||
+ | int32_t (*read_dev)(void *dev, void *buff, uint32_t nb_samples); | ||
+ | int32_t (*write_dev)(void *dev, void *buff, uint32_t nb_samples); | ||
+ | int32_t (*pre_enable)(void *dev, uint32_t mask); | ||
+ | int32_t (*post_disable)(void *dev); | ||
+ | int32_t (*submit)(struct iio_device_data *dev); | ||
+ | int32_t (*trigger_handler)(struct iio_device_data *dev); | ||
+ | int32_t (*debug_reg_read)(void *dev, uint32_t reg, uint32_t *readval); | ||
+ | int32_t (*debug_reg_write)(void *dev, uint32_t reg, uint32_t writeval); | ||
+ | }; | ||
+ | </ | ||
+ | |||
+ | An IIO device can have one (e.g., single channel ADC) or more (e.g., multichannel ADC) channels, so **.num_ch** will be set accordingly. | ||
+ | |||
+ | An IIO device channel defines the channel' | ||
+ | |||
+ | Most of the time, some global (not channel specific) attributes need to be defined through **.attributes**. One example can be the sampling frequency of an ADC, that is most likely device specific, so, by changing it, all the channels will be affected. | ||
+ | |||
+ | **.read_dev** is the device specific function that will be called for filling an IIO buffer with samples. If some additional steps are required before starting the actual capture (e.g., IIO client needs to capture data only from a selection of channels instead of all), a **.pre_enable** function can be implemented. **.post_disable**, | ||
+ | |||
+ | Usually for debug purposes, **.debug_reg_read** and **.debug_reg_write** can expose low level device register access. | ||
+ | |||
+ | Once an **struct iio_device** is available, an application specific **struct iio_device_init** should be defined: | ||
+ | |||
+ | < | ||
+ | struct iio_device_init { | ||
+ | char *name; | ||
+ | void *dev; | ||
+ | struct iio_device *dev_descriptor; | ||
+ | int8_t *raw_buf; | ||
+ | uint32_t raw_buf_len; | ||
+ | char *trigger_id; | ||
+ | }; | ||
+ | </ | ||
+ | |||
+ | This will link the actual instance of a device (**.dev**) with a corresponding IIO layer (**.dev_descriptor**). If user wants to provide an external buffer to IIO, this can be done here too (**.raw_buf**); | ||
+ | |||
+ | The last step before initializing the entire IIO framework by calling **iio_init()** is the definition of a **struct iio_init_param**: | ||
+ | |||
+ | < | ||
+ | struct iio_init_param { | ||
+ | enum pysical_link_type phy_type; | ||
+ | union { | ||
+ | struct no_os_uart_desc *uart_desc; | ||
+ | struct tcp_socket_init_param *tcp_socket_init_param; | ||
+ | }; | ||
+ | struct iio_device_init *devs; | ||
+ | uint32_t nb_devs; | ||
+ | struct iio_trigger_init *trigs; | ||
+ | uint32_t nb_trigs; | ||
+ | }; | ||
+ | </ | ||
+ | |||
+ | In addition to the list of all the IIO devices to get registered (**.devs**) and their number (**.nb_devs**), | ||
+ | Having a **struct iio_init_param**, | ||
+ | |||
+ | Next, **iio_step()** can listen/ | ||
+ | |||
+ | **iio_app_run()** is an example of using what it was described so far (it calls **iio_init()** and **iio_step()**). |