This is an old revision of the document!
The GPIO framework provides a way to handle General-Purpose Input/Output (GPIO) pins when using the No-OS platform drivers.
The GPIO interface documentation is generated using the Doxygen tool and it is available at:
/* GPIO Description declaration */ struct no_os_gpio_desc *gpio_desc; /* GPIO Initialization Parameters */ struct no_os_gpio_init_param gpio_param = { /** Port number */ .port = 0, /** Pull up/down resistor configuration */ .pull = NO_OS_PULL_NONE, /** GPIO Number */ .number = GPIO_1, /** GPIO platform specific functions (Xilinx Platform in this particular example) */ .platform_ops = &xil_gpio_ops, /** GPIO extra parameters (device specific) */ .extra = &xil_gpio_param }; /* Obtain the GPIO decriptor. */ ret = no_os_gpio_get(&gpio_desc, &gpio_param); if (ret) return -1; /* Free the resources allocated by no_os_gpio_get(). */ ret = no_os_gpio_remove(gpio_desc); if (ret) return -1;
Alternatively, if the a specific gpio is optional, the `no_os_gpio_get_optional` function can be used instead of `no_os_gpio_get`.
/* Enable the input direction of the specified GPIO. */ ret = no_os_gpio_direction_input(gpio_desc); if (ret) return -1; /* Enable the output direction of the specified GPIO with logic level high. */ ret = no_os_gpio_direction_output(gpio_desc, NO_OS_GPIO_HIGH); if (ret) return -1; /* Enable the output direction of the specified GPIO with logic level low. */ ret = no_os_gpio_direction_output(gpio_desc, NO_OS_GPIO_LOW); if (ret) return -1; /* Get the direction of the specified GPIO. */ uint8_t dir; ret = no_os_gpio_get_direction(gpio_desc, &dir); if (ret) return -1; /* Set the value of the specified GPIO with logic level high. */ ret = no_os_gpio_set_value(gpio_desc, NO_OS_GPIO_HIGH); if (ret) return -1; /* Set the value of the specified GPIO with logic level low. */ ret = no_os_gpio_set_value(gpio_desc, NO_OS_GPIO_LOW); if (ret) return -1; /* Get the value of the specified GPIO. */ enum no_os_gpio_values val; ret = no_os_gpio_get_value(gpio_desc, &val); if (ret) return -1;