This is an old revision of the document!
DAC_DMA_EXAMPLE is a standard example that sends a sinewave on Tx channels using DMA from a lookup table. If you physically loopback a Tx channel to an Rx channel via an electrical wire, you may run the DAC_DMA_EXAMPLE and read the received data at Rx from particular memory address.
To build the DAC_DMA_EXAMPLE demo, edit the Makefile and add -DDAC_DMA_EXAMPLE to CFLAGS and rebuild. Alternatively, you may simply add a #define DAC_DMA_EXAMPLE in a suitable place in code and rebuild.
To run the DAC_DMA_EXAMPLE, you simply need to run the application as usual by:
The application will eventually print something like this:
DAC_DMA_EXAMPLE: address=0x7f170 samples=65536 channels=4 bits=16
This means that the memory address where the data at Rx is stored is 0x7f170, there are in total 65536 samples, 16-bit wide across 4 channels, which is equivalent to 16384, 16-bit samples per channel.
At this point you may use a Tcl script to retrieve data from memory and store it into .csv files for processing:
xsct legacy/scripts/xilinx_capture.tcl ZYNQ_PS7 0x7f170 65536 4 16 # for Zynq-7000 xsct legacy/scripts/xilinx_capture.tcl ZYNQ_PSU 0x7f170 65536 4 16 # for ZynqMP