This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:fpga:xilinx:pmod:adxrs453_adxl345_lx9 [10 Dec 2012 15:57] – Download Wrapper Alexandru.Tofan | resources:fpga:xilinx:pmod:adxrs453_adxl345_lx9 [29 Mar 2013 11:00] – [Running Demo (SDK) Program] Alexandru.Tofan | ||
---|---|---|---|
Line 15: | Line 15: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <note tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http:// | + | <WRAP tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http:// |
- | </note> | + | </WRAP> |
- | To begin, connect the PmodGYRO2 to J5 connector of LX9 board, pins 7 to 12 (see image below). You must use an extension cable or the [[http:// | + | To begin, connect the PmodGYRO2 to J5 connector of LX9 board, pins 7 to 12. You must use an extension cable or the [[http:// |
{{: | {{: | ||
Line 32: | Line 32: | ||
On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.\\ | On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.\\ | ||
- | <note important> | + | <WRAP important> |
* Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH. | * Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH. | ||
* Connecting the PmodACL to the board with an extension cable provides ease of use. | * Connecting the PmodACL to the board with an extension cable provides ease of use. | ||
* UART must be set to 57600 baudrate. | * UART must be set to 57600 baudrate. | ||
- | </note> | + | </WRAP> |
===== Downloads ===== | ===== Downloads ===== |