This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:fpga:xilinx:pmod:adxrs453_adxl345_lx9 [29 Mar 2013 11:00] – [Running Demo (SDK) Program] Alexandru.Tofan | resources:fpga:xilinx:pmod:adxrs453_adxl345_lx9 [12 Apr 2013 15:43] – [Running Demo (SDK) Program] Lucian Sin | ||
---|---|---|---|
Line 15: | Line 15: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http:// | + | < |
+ | \\ | ||
+ | If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http:// | ||
</ | </ | ||
Line 32: | Line 34: | ||
On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.\\ | On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.\\ | ||
- | <WRAP important> | + | < |
* Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH. | * Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH. | ||
* Connecting the PmodACL to the board with an extension cable provides ease of use. | * Connecting the PmodACL to the board with an extension cable provides ease of use. | ||
Line 39: | Line 41: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
+ | \\ | ||
{{: | {{: | ||
</ | </ |