This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:adxrs453 [20 Nov 2015 13:48] – hide linux, it is not supported at the moment Lars-Peter Clausen | resources:fpga:xilinx:pmod:adxrs453 [08 Feb 2021 13:49] (current) – Change broken link Iulia Moldovan | ||
---|---|---|---|
Line 8: | Line 8: | ||
* A design which shows how to acquire data from the ADXRS453 Gyroscope. | * A design which shows how to acquire data from the ADXRS453 Gyroscope. | ||
* **HW Platform(s): | * **HW Platform(s): | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 14: | Line 14: | ||
* A design which demonstrates how to acquire data and display it using Digilent PmodGYRO2 and PmodACL. Data acquired from PmodGYRO2 is displayed in Degrees per Second, and data acquired from PmodACL is displayed in g. Data is formatted in 4 columns. | * A design which demonstrates how to acquire data and display it using Digilent PmodGYRO2 and PmodACL. Data acquired from PmodGYRO2 is displayed in Degrees per Second, and data acquired from PmodACL is displayed in g. Data is formatted in 4 columns. | ||
* **HW Platform(s): | * **HW Platform(s): | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 25: | Line 25: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 37: | Line 37: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | ||
If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | ||
Line 131: | Line 131: | ||
**Avnet ZedBoard: | **Avnet ZedBoard: | ||
* [[https:// | * [[https:// | ||
- | * [[https:// | + | * [[https:// |
- | * [[https:// | + | * [[https:// |
- | * [[https:// | + | * [[https:// |
| | ||
</ | </ | ||
Line 144: | Line 144: | ||
In order to prepare the SD Card for booting Linux on the ZedBoard: | In order to prepare the SD Card for booting Linux on the ZedBoard: | ||
- | * Download the device tree: [[https:// | + | * Download the device tree: [[https:// |
* Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step | ||
- | * [[http:// | + | * [[/ |
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. |