This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:adxl345 [30 Oct 2013 09:56] – [Preparing the SD Card] Alexandru.Tofan | resources:fpga:xilinx:pmod:adxl345 [09 Jan 2021 00:57] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 6: | Line 6: | ||
**HW Platform(s): | **HW Platform(s): | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 15: | Line 15: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 27: | Line 27: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | ||
If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | ||
Line 151: | Line 151: | ||
| | ||
</ | </ | ||
+ | <wrap hide> | ||
====== Linux Device Driver ====== | ====== Linux Device Driver ====== | ||
Line 160: | Line 160: | ||
In order to prepare the SD Card for booting Linux on the ZedBoard: | In order to prepare the SD Card for booting Linux on the ZedBoard: | ||
* Download the device tree: [[https:// | * Download the device tree: [[https:// | ||
- | * Configure the kernel to include the driver for the ADXL345: [[http:// | + | * Configure the kernel to include the driver for the ADXL345: [[/ |
* Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step and the kernel configuration above | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step and the kernel configuration above | ||
- | * [[http:// | + | * [[/ |
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
Line 217: | Line 217: | ||
{{: | {{: | ||
+ | </ | ||
===== More information ===== | ===== More information ===== | ||
* [[ez> | * [[ez> | ||
* Example questions: {{rss> | * Example questions: {{rss> |