This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:xilinx:pmod:adxl345 [30 Oct 2013 09:56] – [Preparing the SD Card] Alexandru.Tofan | resources:fpga:xilinx:pmod:adxl345 [20 Nov 2015 13:40] – hide linux, it is not supported at the moment Lars-Peter Clausen | ||
---|---|---|---|
Line 151: | Line 151: | ||
| | ||
</ | </ | ||
+ | <wrap hide> | ||
====== Linux Device Driver ====== | ====== Linux Device Driver ====== | ||
Line 162: | Line 162: | ||
* Configure the kernel to include the driver for the ADXL345: [[http:// | * Configure the kernel to include the driver for the ADXL345: [[http:// | ||
* Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step and the kernel configuration above | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step and the kernel configuration above | ||
- | * [[http:// | + | * [[http:// |
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
Line 217: | Line 217: | ||
{{: | {{: | ||
+ | </ | ||
===== More information ===== | ===== More information ===== | ||
* [[ez> | * [[ez> | ||
* Example questions: {{rss> | * Example questions: {{rss> |