This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:xilinx:pmod:adt7420 [05 Sep 2013 20:59] – [Avnet ZedBoard] Andrei Cozma | resources:fpga:xilinx:pmod:adt7420 [09 Jan 2021 00:57] – user interwiki links Robin Getz | ||
---|---|---|---|
Line 13: | Line 13: | ||
**HW Platform(s): | **HW Platform(s): | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 22: | Line 22: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 33: | Line 33: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | ||
If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | ||
Line 127: | Line 127: | ||
</ | </ | ||
+ | <WRAP round important 80%> | ||
+ | When using the ZedBoard reference design in order to develop your own software, please make sure that the following options are set in " | ||
+ | |||
+ | <code c> | ||
+ | // Select between PS7 or AXI Interface | ||
+ | #define USE_PS7 1 | ||
+ | // SPI used in the design | ||
+ | #define USE_SPI 0 | ||
+ | // I2C used in the design | ||
+ | #define USE_I2C 1 | ||
+ | // Timer (+interrupts) used in the design | ||
+ | #define USE_TIMER 0 | ||
+ | // External interrupts used in the design | ||
+ | #define USE_EXTERNAL | ||
+ | // GPIO used in the design | ||
+ | #define USE_GPIO | ||
+ | </ | ||
+ | |||
+ | </ | ||
===== Downloads ===== | ===== Downloads ===== | ||
Line 140: | Line 159: | ||
* [[https:// | * [[https:// | ||
* [[https:// | * [[https:// | ||
- | * [[https:// | + | * [[https:// |
* [[https:// | * [[https:// | ||
| |