This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:ad7980 [20 Nov 2015 13:42] – hide linux, it is not supported at the moment Lars-Peter Clausen | resources:fpga:xilinx:pmod:ad7980 [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 6: | Line 6: | ||
**HW Platform(s): | **HW Platform(s): | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 15: | Line 15: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 26: | Line 26: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | ||
If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | ||
Line 112: | Line 112: | ||
| | ||
</ | </ | ||
- | < | + | < |
====== Linux Device Driver - Custom HDL PCore ====== | ====== Linux Device Driver - Custom HDL PCore ====== | ||
Line 125: | Line 125: | ||
* Download the project libraries: [[https:// | * Download the project libraries: [[https:// | ||
* Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step | * Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step | ||
- | * [[http:// | + | * [[/ |
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
Line 186: | Line 186: | ||
Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | ||
- | * [[http:// | + | * [[/ |
Launch the ADI IIO Oscilloscope. | Launch the ADI IIO Oscilloscope. |