This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:ad7980 [25 May 2012 12:46] – [More information] Andrei Cozma | resources:fpga:xilinx:pmod:ad7980 [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 5: | Line 5: | ||
The [[adi> | The [[adi> | ||
- | **HW Platform(s): | + | **HW Platform(s): |
- | **System:** Microblaze, AXI, UART \\ | + | * [[xilinx>products/ |
+ | | ||
+ | | ||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
Line 12: | Line 15: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
+ | * [[http:// | ||
+ | * [[http:// | ||
* [[http:// | * [[http:// | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). |
- | * A UART terminal (Tera Term/ | + | * A UART terminal (Tera Term/ |
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <note tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
- | </note> | + | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// |
- | Extract the project from the archive file (AD7980.zip) to the location | + | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// |
- | To begin, connect the PmodAD4 to J5 connector of LX9 board, pins 1 to 6 (see image below). You can use an extension cable for ease of use. Connect the USB cables | + | ==== Avnet LX9 MicroBoard Setup ==== |
+ | |||
+ | Extract the project from the archive file (AD7980_< | ||
+ | |||
+ | To begin, connect the PmodAD4 to J5 connector of LX9 board, pins 1 to 6 (see image below). You can use an extension cable for ease of use. Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector. | ||
{{: | {{: | ||
- | Start IMPACT, and double click " | + | ==== Digilent Nexys™3 Spartan-6 FPGA Board ==== |
+ | |||
+ | Extract the project from the archive file (AD7980_< | ||
+ | |||
+ | To begin, connect the PmodAD4 to JA connector of Nexys3 board, pins JA1 to JA6 (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ==== Avnet ZedBoard ==== | ||
+ | |||
+ | To begin, connect the PmodAD4 to JD connector of ZedBoard (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ==== FPGA Configuration for Nexys3 and LX-9 MicroBoard ==== | ||
+ | |||
+ | Start IMPACT, and double click " | ||
{{: | {{: | ||
- | If programming was successful, you should be seeing messages appear on the terminal window as shown in the figure below. After programming the AD7980 device, the program will automatically read the value of the analog voltage input and print it via UART. Pressing [Enter] will initialize another conversion. | ||
- | {{: | + | If programming was successful, you should be seeing messages appear on the terminal window as shown in the figure below. After programming the AD7980 device, the program will automatically read the value of the analog voltage input and print it via UART. |
+ | {{: | ||
+ | {{: | ||
+ | ==== FPGA Configuration for ZedBoard ==== | ||
+ | Run the **download.bat** script from the " | ||
+ | The script will automatically configure the ZYNQ SoC and download the *.elf file afterwards. | ||
+ | |||
+ | <WRAP center round tip 80%> | ||
+ | If the download script fails to run, modify the Xilinx Tools path in **download.bat** to match your Xilinx Installation path. | ||
+ | </ | ||
+ | |||
+ | If programming was successful, you should be seeing messages appear on the terminal window. After programming the AD7980 device, the program will automatically read the value of the analog voltage input and print it via UART. | ||
===== Using the reference design ===== | ===== Using the reference design ===== | ||
==== Functional Description ==== | ==== Functional Description ==== | ||
- | The reference design is a custom SPI interface which functions in CS Mode, 3-wire, Without Busy Indicator (see AD7980 datasheet pg. 17). | + | === Avnet LX-9 MicroBoard and Digilent Nexys3 === |
- | The hardware | + | The reference design is a custom |
- | <note important> | + | === Avnet ZedBoard === |
- | * Connecting the PmodAD4 to the LX-9 Board using an extension cable provides ease of use. | + | |
- | * UART must be set to 57600 baudrate. | + | |
- | * The reference voltage for the AD7980 is 2.5V. | + | |
- | </ | + | |
+ | The reference design is a custom SPI interface which functions in CS Mode, 3-wire, Without Busy Indicator (see AD7980 datasheet pg. 17). The software programs the device, and afterwards, using DMA, transfers 8192 samples and prints them via UART. | ||
+ | |||
+ | <WRAP round 80% important> | ||
+ | * Connecting the PmodAD4 to the boards using an extension cable provides ease of use. | ||
+ | * UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard and ZedBoard or 9600 Baud Rate for the Digilent Nexys™3 Board. | ||
+ | * The reference voltage for the AD7980 is 2.5V. | ||
+ | * If you want to use another reference voltage, you will need to modify the VREF definition at the beginning of “main.c”. The range for VREF must be 2.4V ≤ VREF ≤ 5.1V. | ||
+ | * If you want to use AVDD > DVDD (= 3.3V) then JP3 on PmodAD4 must be removed. The range for AVDD is 3.0V ≤ AVDD ≤ 5.5V | ||
+ | </ | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | {{: | ||
+ | <WRAP round download 80%> | ||
+ | \\ | ||
+ | **Avnet LX-9 MicroBoard: **\\ | ||
+ | * {{: | ||
+ | |||
+ | **Digilent Nexys™3: | ||
+ | * {{: | ||
+ | |||
+ | **Avnet ZedBoard: | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | | ||
+ | </ | ||
+ | <wrap hide> | ||
+ | ====== Linux Device Driver - Custom HDL PCore ====== | ||
+ | |||
+ | Connect PmodAD4 to the JD1 connector of the ZedBoard (upper row of pins). | ||
+ | |||
+ | ===== Preparing the SD Card ===== | ||
+ | |||
+ | In order to prepare the SD Card for booting Linux on the ZedBoard: | ||
+ | * Download the device tree: [[https:// | ||
+ | * Download the Xilinx XPS project: [[https:// | ||
+ | * Download the AD7980 IPcore: [[https:// | ||
+ | * Download the project libraries: [[https:// | ||
+ | * Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step | ||
+ | * [[/ | ||
+ | |||
+ | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
+ | If everything is correct, the system should boot up. If you don't have an HDMI monitor, connect to the board via UART, Baud Rate 115200. | ||
+ | |||
+ | There are 2 ways to test the driver. | ||
+ | * Using the terminal window | ||
+ | * Using the ADI IIO Oscilloscope | ||
+ | |||
+ | ===== Using the terminal window ===== | ||
+ | |||
+ | Open a new terminal window by pressing **Ctrl+Alt+T**. | ||
+ | |||
+ | Navigate to the location of the device and identify it using the following commands: | ||
+ | < | ||
+ | cd / | ||
+ | ls | ||
+ | iio:device0 iio:device1 trigger0 | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | AD7980 | ||
+ | </ | ||
+ | |||
+ | If the **cat name** command doesn' | ||
+ | < | ||
+ | cd .. | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | </ | ||
+ | |||
+ | To see the list of options that the AD7980 driver provides, type: | ||
+ | < | ||
+ | ls | ||
+ | buffer | ||
+ | </ | ||
+ | |||
+ | To read the raw input voltage, type: | ||
+ | < | ||
+ | cd buffer | ||
+ | echo 128 > length | ||
+ | echo 1 > enable | ||
+ | hexdump -x / | ||
+ | 0000000 | ||
+ | 0000010 | ||
+ | 0000020 | ||
+ | 0000030 | ||
+ | 0000040 | ||
+ | 0000050 | ||
+ | 0000060 | ||
+ | 0000070 | ||
+ | </ | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The commands written above can also be used if not using an HDMI monitor and a wireless keyboard, by using a serial terminal, and typing the commands after the system boot-up is complete. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ===== Using the ADI IIO Oscilloscope ===== | ||
+ | |||
+ | Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | ||
+ | * [[/ | ||
+ | |||
+ | Launch the ADI IIO Oscilloscope. | ||
+ | |||
+ | Select **AD7980** from the **Device** drop-down menu. Set the desired number of samples in the **Sample Count** tab. Click the **Green Play Button** in order to start capturing and displaying data. Click **Stop** to stop the process. | ||
+ | {{: | ||
+ | </ | ||
===== More information ===== | ===== More information ===== | ||
* [[ez> | * [[ez> | ||
* Example questions: {{rss> | * Example questions: {{rss> |