Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:fpga:xilinx:pmod:ad7476a [20 Nov 2015 13:34] – hide linux, it is not supported at the moment Lars-Peter Clausen | resources:fpga:xilinx:pmod:ad7476a [27 Nov 2017 10:42] – s/PmodACL/PmodAD1/ Lars-Peter Clausen |
---|
* [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]] | * [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]] |
* [[http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx|Avnet ZedBoard]] | * [[http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx|Avnet ZedBoard]] |
* [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL (Digilent)]] | * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-AD1|PmodAD1 (Digilent)]] |
| |
==== Required Software ==== | ==== Required Software ==== |
Extract the project from the archive file (AD7476A_<board_name>.zip) to the location you desire. | Extract the project from the archive file (AD7476A_<board_name>.zip) to the location you desire. |
| |
To begin, connect the PmodACL to J5 connector of LX9 board (see image below). You can use an extension cable for ease of use. Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector. | To begin, connect the PmodAD1 to J5 connector of LX9 board (see image below). You can use an extension cable for ease of use. Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector. |
| |
{{:resources:fpga:xilinx:pmod:pmodad1.jpg?200|PmodAD1 and LX-9}} | {{:resources:fpga:xilinx:pmod:pmodad1.jpg?200|PmodAD1 and LX-9}} |
Extract the project from the archive file (AD7476A_<board_name>.zip) to the location you desire. | Extract the project from the archive file (AD7476A_<board_name>.zip) to the location you desire. |
| |
To begin, connect the PmodACL to JA connector of NEXYS3 board (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). | To begin, connect the PmodAD1 to JA connector of NEXYS3 board (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). |
| |
{{:resources:fpga:xilinx:pmod:pmodad1_nexys3.jpg?200|PmodAD1 and Nexys™3}} | {{:resources:fpga:xilinx:pmod:pmodad1_nexys3.jpg?200|PmodAD1 and Nexys™3}} |