This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:ad7303 [20 Nov 2015 13:44] – Lars-Peter Clausen | resources:fpga:xilinx:pmod:ad7303 [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 9: | Line 9: | ||
* A design which shows how to used the **AD7303 DAC** by outputting square and a sawtooth waveforms | * A design which shows how to used the **AD7303 DAC** by outputting square and a sawtooth waveforms | ||
* **HW Platform(s): | * **HW Platform(s): | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 26: | Line 26: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 37: | Line 37: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | ||
If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | ||
Line 182: | Line 182: | ||
* Download the device tree: [[https:// | * Download the device tree: [[https:// | ||
* Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step | ||
- | * [[http:// | + | * [[/ |
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
Line 242: | Line 242: | ||
Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | ||
- | * [[http:// | + | * [[/ |
Launch the ADI IIO Oscilloscope. | Launch the ADI IIO Oscilloscope. | ||
Line 274: | Line 274: | ||
====== AD7303 Pmod and AD7476 Pmod Reference Design ====== | ====== AD7303 Pmod and AD7476 Pmod Reference Design ====== | ||
{{page> | {{page> | ||
- | < | + | </wrap> |
====== More information ====== | ====== More information ====== | ||
* [[ez> | * [[ez> | ||
* Example questions: {{rss> | * Example questions: {{rss> |