This is an old revision of the document!
The AD5933 is a high precision impedance converter system solution that combines an on-board frequency generator with a 12-bit, 1 MSPS, analog-to-digital converter (ADC). The frequency generator allows an external complex impedance to be excited with a known frequency. The response signal from the impedance is sampled by the on-board ADC and a discrete Fourier transform (DFT) is processed by an on-board DSP engine. The DFT algorithm returns a real (R) and imaginary (I) data-word at each output frequency. Once calibrated, the magnitude of the impedance and relative phase of the impedance at each frequency point along the sweep is easily calculated. This is done off chip using the real and imaginary register contents, which can be read from the serial I2C interface.
HW Platform(s):
The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT).
If you are not familiar with LX9 and/or Xilix tools, please visit
http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm for details.
If you are not familiar with Nexys™3 and/or Xilix tools, please visit
http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3 for details.
If you are not familiar with ZedBoard and/or Xilix tools, please visit
http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx for details.
Extract the project from the archive file (AD5933_<board_name>.zip) to the location you desire.
To begin, connect the PmodIA to J5 connector of LX9 board, pins 3 to 6 (see image below). You must use an extension cable. . Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector.
Extract the project from the archive file (AD5933_<board_name>.zip) to the location you desire.
To begin, connect the PmodIA to JA connector of Nexys™3 board, pins JA3 to JA6 (see image below). You must use an extension cable. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART).
To begin, connect the PmodIA to JC1 connector of ZedBoard (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART).
Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Start a UART terminal (set to appropiate baud rate) and then program the device using the bit file provided in the project *.zip archive, located in the “sw” folder (../ad5933/sw/AD5933.bit).
Run the download.bat script from the “../bin” folder downloaded from the github (see the links in the download section of the wiki page). The script will automatically configure the ZYNQ SoC and download the *.elf file afterwards.
If the download script fails to run, modify the Xilinx Tools path in download.bat to match your Xilinx Installation path.
If programming was successful, you should be seeing messages appear on the terminal window as shown in the figures below. After programming the AD5933 device, the program will automatically read the temperature value of the AD5933. Afterwards it will start a calibration process. Use a 47 Kohm resistor for this purpose. After calibration is complete, the user will be promped to change the 47 Kohm resistor with the desired component for measurement, and press [Enter] afterwards. The result of the measurement will be printed on the terminal window both in ohms and Kohms.
The reference design is a consists of an IIC interface between the FPGA and the PmodIA. Functions for setting the frequency sweeps and other parameters can be found in AD5933.c, in the “sw” folder (../ad5933/sw/AD5933.c). If you desire to use another resistor for calibration purposes, you must change the “47000” parameter for the AD5933_CalculateGainFactor function in main.c with the value of your resistor.
When using the ZedBoard reference design in order to develop your own software, please make sure that the following options are set in “system_config.h”:
// Select between PS7 or AXI Interface #define USE_PS7 1 // SPI used in the design #define USE_SPI 1 // I2C used in the design #define USE_I2C 0 // Timer (+interrupts) used in the design #define USE_TIMER 0 // External interrupts used in the design #define USE_EXTERNAL 0 // GPIO used in the design #define USE_GPIO 0
If you encounter a compilation error regarding functions from “math.h”, please follow the answer from Xilinx in order to enable the Math Libraries: http://www.xilinx.com/support/answers/52971.htm
Avnet LX-9 MicroBoard:
Digilent Nexys™3:
Avnet ZedBoard:
====== Linux Device Driver ====== Connect PmodIA to the JC1 connector of the ZedBoard (upper row of pins). ===== Preparing the SD Card ===== In order to prepare the SD Card for booting Linux on the ZedBoard: * Download the device tree: PmodIA Linux devicetree * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step * Linux with HDMI video output on the ZED and ZC702. Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. If everything is correct, the system should boot up. If you don't have an HDMI monitor, connect to the board via UART, Baud Rate 115200. There are 2 ways to test the driver. * Using the terminal window * Using the ADI IIO Oscilloscope ===== Using the terminal window ===== Open a new terminal window by pressing Ctrl+Alt+T. Navigate to the location of the device and identify it using the following commands: <code> cd /sys/bus/iio/devices/ ls iio:device0 iio:device1 cd iio\:device0 cat name ad5933 </code> If the cat name command doesn't return ad5933, then change the number of the iio:device, and check again. <code> cd .. cd iio\:device1 cat name </code> To see the list of options that the AD5933 driver provides, type: <code> ls buffer out_voltage0_freq_increment power dev out_voltage0_freq_points scan_elements in_temp0_input out_voltage0_freq_start subsystem in_voltage0_scale out_voltage0_scale uevent in_voltage0_scale_available out_voltage0_scale_available name out_voltage0_settling_cycles </code> ===Set sweep start frequency=== Description: Frequency sweep start frequency in Hz. <code> echo 15000 > out_voltage0_freq_start cat out_voltage0_freq_start 14999 </code> ===Set frequency increment=== Description: Frequency increment in Hz (step size) between consecutive frequency points along the sweep. <code> echo 200 > out_voltage0_freq_increment </code> ===Set number of frequency points=== Description: Number of frequency points (steps) in the frequency sweep. This value, in conjunction with the outY_freq_start and the outY_freq_increment, determines the frequency sweep range for the sweep operation. <code> echo 100 > out_voltage0_freq_points cat out_voltage0_freq_points 100 </code> ===Set number of settling time cycles=== Description: Number of output excitation cycles (settling time cycles) that are allowed to pass through the unknown impedance, after each frequency increment, and before the ADC is triggered to perform a conversion sequence of the response signal. <code> echo 15 > out_voltage0_settling_cycles cat out_voltage0_settling_cycles 15 </code> ===Show available output ranges=== Description: List available output scales/ranges in millivolt. <code> cat out_voltage0_scale_available 1980 970 383 198 </code> ===Set output range=== Description: Sets output scale/range in millivolt. <code> echo 1980 > out_voltage0_scale cat out_voltage0_scale 1980 </code> ===Show available input scales=== Description: List available input scales. Programmable gain amplifier (PGA) options. <code> cat in_voltage0_scale_available 1 0.2 </code> ===Set input scale=== Description: Sets input scale. Controls programmable gain amplifier (PGA). <code> echo 0.2 > in_voltage0_scale cat in_voltage0_scale 0.2 </code> ===Show internal temperature=== Description: Shows temperature in milli degrees Celsius. The on-chip temperature sensor allows an accurate measurement of the ambient device temperature. The measurement range of the sensor is −40°C to +125°C. <code> cat in_temp0_input 25062 </code> ===Buffer Management=== The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer. Every buffer implementation features a set of files: <code> cd buffer ls enable length </code> length Get/set the number of sample sets that may be held by the buffer. enable Enables/disables the buffer. This file should be written last, after length and selection of scan elements. <code> cd scan_elements ls in_voltage0_imag_raw_en in_voltage0_real_raw_en in_voltage0_imag_raw_index in_voltage0_real_raw_index in_voltage0_imag_raw_type in_voltage0_real_raw_type </code> scan_elements The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer. <code> grep “” * in_voltage0_imag_raw_en:1 in_voltage0_imag_raw_index:1 in_voltage0_imag_raw_type:le:s16/16»0 in_voltage0_real_raw_en:1 in_voltage0_real_raw_index:0 in_voltage0_real_raw_type:le:s16/16»0 </code> ====Buffer Example==== <code> echo 15000 > out_voltage0_freq_start echo 200 > out_voltage0_freq_increment echo 100 > out_voltage0_freq_points echo 512 > buffer/length echo 1 > buffer/enable </code> ==== Data interpretation ==== ^ index ^ datum ^ type ^ | 0 | Real Sample f0 | signed short 16-bit | | 1 | Imag Sample f0 | signed short 16-bit | | [fn * 2] | Real Sample fn | signed short 16-bit | | [fn * 2] + 1 | Imag Sample fn | signed short 16-bit | Z = in_voltage0_real_raw + i * in_voltage0_imag_raw The commands written above can also be used if not using an HDMI monitor and a wireless keyboard, by using a serial terminal, and typing the commands after the system boot-up is complete.