This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:fpga:xilinx:kc705:adv7511 [10 Nov 2014 14:52] – [Supported Carriers] Lucian Sin | resources:fpga:xilinx:kc705:adv7511 [15 Jul 2015 16:09] – change adv7511 new platform and new hardware project pictures and explinations and added ZED library to library section Lucian Sin | ||
---|---|---|---|
Line 25: | Line 25: | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * Xilinx | + | * Xilinx |
- | * A UART terminal (Tera Term/ | + | * A UART terminal (Tera Term/ |
- | * For ISE, Baud rate 57600 for AC701/ | + | |
- | * For Vivado, Baud rate 115200 for AC701/ | + | |
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
Line 36: | Line 34: | ||
Run the **// | Run the **// | ||
- | **Note: | + | **Note: |
If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | ||
Line 112: | Line 110: | ||
* Go to // | * Go to // | ||
{{ : | {{ : | ||
- | * Use a new hardware platform, so choose //**Create new**// in // | + | * Use a new hardware platform, so choose //**New**// in //**Target |
{{ : | {{ : | ||
- | * In //**Target Hardware Specification**// browse the location of //**SDK_Export\hw\system.xml**// and click //**Finish**// | + | * At the **Target Hardware Specification** |
{{ : | {{ : | ||
* Then give a name to the project and click // | * Then give a name to the project and click // | ||
Line 122: | Line 120: | ||
* Now the project without source code looks like this | * Now the project without source code looks like this | ||
{{ : | {{ : | ||
- | * Then the no-OS software for the used FPGA board must be added from Github. Also the library must be added (ZC library for a Zynq based platform or Microblaze library for AC701, | + | * Then the no-OS software for the used FPGA board must be added from Github. Also the library must be added (ZC library for a Zynq based platform(except ZED), ZED library for a ZED platform or Microblaze library for AC701, |
{{ : | {{ : | ||
* Afterwards click right on project name and go to // | * Afterwards click right on project name and go to // | ||
Line 130: | Line 128: | ||
* In the same window, go to // | * In the same window, go to // | ||
{{ : | {{ : | ||
- | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the Console window will display | + | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the Console window will display the result of the build. If the build is not done automatically select the // |
{{ : | {{ : | ||
* At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. You can program the FPGA by going to //**Xilinx Tools**//. | * At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. You can program the FPGA by going to //**Xilinx Tools**//. | ||
Line 163: | Line 161: | ||
The HDL Reference Designs and the no-OS Software can be downloaded from the Analog Devices Github.\\ | The HDL Reference Designs and the no-OS Software can be downloaded from the Analog Devices Github.\\ | ||
\\ | \\ | ||
- | <WRAP round important 80%> | ||
- | \\ | ||
- | The software project contains 2 components: the Reference Design files and the ADV7511 Transmitter Library. All the components have to be downloaded from the links below. | ||
- | </ | ||
**Evaluation Scripts:** | **Evaluation Scripts:** | ||
Line 180: | Line 174: | ||
**HDL Reference Designs:** | **HDL Reference Designs:** | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
- | | + | Release hdl_2014_r2: |
- | * **KC705 HDL Reference Design for Vivado: ** https:// | + | \\ |
- | * **vC707 HDL Reference Design for Vivado: ** https:// | + | |
- | * **ZC702 HDL Reference Design for Vivado: ** https:// | + | * **KC705 HDL Reference Design for Vivado: ** https:// |
- | * **ZC706 HDL Reference Design for Vivado: ** https:// | + | * **vC707 HDL Reference Design for Vivado: ** https:// |
- | * **ZED HDL Reference Design for Vivado: ** https:// | + | * **ZC702 HDL Reference Design for Vivado: ** https:// |
+ | * **ZC706 HDL Reference Design for Vivado: ** https:// | ||
+ | * **ZED HDL Reference Design for Vivado: ** https:// | ||
</ | </ | ||
**no-OS Software:** | **no-OS Software:** | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
- | | + | Release 2014_R2: |
- | * **ADV7511 AC701 Reference Design: ** https:// | + | \\ |
- | * **ADV7511 KC705 Reference Design: ** https:// | + | |
- | * **ADV7511 VC707 Reference Design: ** https:// | + | * **ADV7511 AC701 Reference Design: ** https:// |
- | * **ADV7511 ZC Library: ** https:// | + | * **ADV7511 KC705 Reference Design: ** https:// |
- | * **ADV7511 ZC702 Reference Design: ** https:// | + | * **ADV7511 VC707 Reference Design: ** https:// |
- | * **ADV7511 ZC706 Reference Design: ** https:// | + | * **ADV7511 ZC Library: ** https:// |
- | * **ADV7511 ZedBoard Library: ** https:// | + | * **ADV7511 ZC702 Reference Design: ** https:// |
- | * **ADV7511 ZedBoard Reference Design: ** https:// | + | * **ADV7511 ZC706 Reference Design: ** https:// |
+ | * **ADV7511 ZedBoard Library: ** https:// | ||
+ | * **ADV7511 ZedBoard Reference Design: ** https:// | ||
</ | </ | ||
<WRAP round help 80%> | <WRAP round help 80%> | ||
- | \\ | ||
* Questions? [[http:// | * Questions? [[http:// | ||
</ | </ | ||
- | ===== Tar file contents ===== | ||
- | |||
- | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http:// | ||
- | |||
- | | license.txt | ADI license & copyright information. | | ||
- | | system.mhs | ||
- | | system.xmp | ||
- | | data/ | UCF file and/or DDR MIG project files. | | ||
- | | docs/ | Documentation files (Please note that this wiki page is the documentation for the reference design). | | ||
- | | sw/ | Software (Xilinx SDK) & bit file(s). | | ||
- | | cf_lib/ | ||
- | |||
===== More information ===== | ===== More information ===== |