This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:terminal_common [02 Jul 2013 09:22] – [Hardware Setup] Istvan Csomortani | resources:fpga:xilinx:interposer:terminal_common [02 Jul 2013 12:02] – Correct typeos Istvan Csomortani | ||
---|---|---|---|
Line 10: | Line 10: | ||
* Power the ADI evaluation board. | * Power the ADI evaluation board. | ||
- | At this point everything is set up and it is possible to start the evaluation of the ADI hardware through an UART terminal. | ||
===== Configure Tera Term ===== | ===== Configure Tera Term ===== | ||
Line 23: | Line 22: | ||
{{ : | {{ : | ||
+ | |||
+ | After the configuration of the terminal was finished, the software application has to be uploaded and started on the configured system. This can be done by running the // | ||
+ | |||
+ | <WRAP tip>If the script threw an error, verify if the Xilinx EDK path specified in the **Loadapp.bat** script is corresponding with the current install path. If not change it to the correct one.</ |