This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:cn0271 [16 Jul 2012 15:21] – Approved Andrei Cozma | resources:fpga:xilinx:interposer:cn0271 [31 Dec 2020 06:01] – fix link Robin Getz | ||
---|---|---|---|
Line 5: | Line 5: | ||
* [[adi> | * [[adi> | ||
- | ===== Evaluation Boards | + | ===== Reference Circuits |
- | + | ||
- | * [[adi> | + | |
+ | * [[adi> | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * a compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
- | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-CN0271A-SDPZ** Evaluation Board. | + | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-CN0271-SDPZ** Evaluation Board. |
{{ : | {{ : | ||
Line 38: | Line 33: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[adi>/ | + | * [[adi> |
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 54: | Line 48: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
+ | * The EVAL-CN0271 reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | + | <WRAP round download 80%> | |
- | * {{:resources: | + | \\ |
- | + | * **AD7790 Driver:** https://github.com/ | |
- | The following table presents a short description the reference design archive contents. | + | * **CN0271 Commands:** https:// |
- | + | | |
- | ^ **Folder** ^ **Description** ^ | + | * **EDK KC705 Reference |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | \\ |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | </ |
- | | Software | Contains the source files of the software | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | | + | |
====== Run the Demonstration Project ====== | ====== Run the Demonstration Project ====== | ||
- | {{page> | + | ===== Hardware setup ===== |
- | ===== Demonstration Project User Interface ===== | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. | ||
+ | </ | ||
- | The following figure presents | + | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. |
+ | | ||
- | {{ : | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-CN0271 reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **adcCode? | ||
+ | | **temperature? | ||
+ | | **reset!** | Resets the serial interface with AD7790. | | ||
- | The communication with the board is activated / deactivated by toggling the **// | ||
- | Data acquired from the AD7790 is plotted in the Graph Window, and the current temperature that is being read is displayed in the Numeric Display located in the bottom left of the graph. | + | Commands can be executed using a serial terminal connected to the UART peripheral |
- | ===== Troubleshooting ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ : | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | ===== Software Project Setup ===== |
- | * Check that the evaluation board is powered as instructed in the board' | + | {{page> |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |