Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:fpga:xilinx:interposer:cn0188 [22 Feb 2012 13:51] – Added the EVAL-CN0188-SDPZ board's image and the zip file. Dragos Bogdan | resources:fpga:xilinx:interposer:cn0188 [23 Feb 2012 14:04] – Replaced EVAL-AD5172SDZ with the correct name of the board (Overview), Dragos Bogdan |
---|
====== Overview ====== | ====== Overview ====== |
| |
This document presents the steps to setup an environment for using the **[[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]]** evaluation board together with the Xilinx KC705 FPGA board, the Xilinx Embedded Development Kit (EDK) and the [[http://micrium.com/page/products/tools/probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5172SDZ Evaluation Board with the Xilinx KC705 board. | This document presents the steps to setup an environment for using the **[[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]]** evaluation board together with the Xilinx KC705 FPGA board, the Xilinx Embedded Development Kit (EDK) and the [[http://micrium.com/page/products/tools/probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-CN0188-SDPZ Evaluation Board with the Xilinx KC705 board. |
| |
{{ :resources:fpga:xilinx:interposer:cn0188.jpg?600 }} | {{ :resources:fpga:xilinx:interposer:cn0188.jpg?600 }} |