This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:fpga:xilinx:interposer:adf4106 [26 Jul 2012 13:19] – created Alexandru.Tofan | resources:fpga:xilinx:interposer:adf4106 [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
- | * [[adi> | + | * [[adi>EVAL-ADF4106|EVAL-ADF4106SD1Z]] |
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
- | {{ : | + | {{ : |
For component evaluation and performance purposes, as opposed to quick prototyping, | For component evaluation and performance purposes, as opposed to quick prototyping, | ||
Line 28: | Line 27: | ||
* [[adi> | * [[adi> | ||
* [[adi>/ | * [[adi>/ | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
- | * [[http:// | + | |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 37: | Line 35: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-ADF4106SD1Z** evaluation board | * **EVAL-ADF4106SD1Z** evaluation board | ||
Line 43: | Line 41: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
===== Downloads ===== | ===== Downloads ===== | ||
- | | + | <WRAP round download 80%> |
- | + | \\ | |
- | The following table presents a short description the reference design archive contents. | + | * **ADF4106 Driver:** https://github.com/ |
- | + | * **ADF4106 Commands:** https:// | |
- | ^ **Folder** ^ **Description** ^ | + | |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | * **EDK KC705 Reference project:** https:// |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | \\ |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | </ |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microblaze memory. | | + | |
- | + | ||
- | ====== Run the Demonstration Project ====== | + | |
- | + | ||
- | {{page> | + | |
- | + | ||
- | ===== Demonstration Project User Interface ===== | + | |
- | + | ||
- | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-ADF4106SD1Z** evaluation board. | + | |
- | + | ||
- | {{ : | + | |
- | **Section A** allows for the communication with the board to be activated / deactivated by toggling the //ON/OFF// switch. The // | + | ===== Hardware setup ===== |
- | **Sections B, C and D** allow for configuration | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage | ||
+ | </ | ||
- | **Section B** allows for the configuration of the //Reference Counter Latch//. The //LDP// switch allows setting | + | |
+ | * Connect | ||
- | **Section C** allows for the configuration of the //N Counter Latch//. The //CP Gain// switch allows toggling between different settings for the charge pump. The //B Slider// allows setting the B Counter | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-ADF4106SD1Z reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **register=** | Update | ||
+ | | **register? | ||
+ | | **frequency=** | Set the VCO frequency. Accepted value:\\ 5 .. 6000 - betwwen 5Mhz and 6Ghz | | ||
+ | | **frequency? | ||
- | **Sections D** allows programming both the // | + | Commands |
- | ===== Troubleshooting ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ : | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | ===== Software Project Setup ===== |
- | * Check that the evaluation board is powered as instructed in the board' | + | {{page> |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |