This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:interposer:adf4106 [19 Nov 2012 18:57] – [Evaluation Boards] fix link Lars-Peter Clausen | resources:fpga:xilinx:interposer:adf4106 [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 10: | Line 10: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
Line 27: | Line 27: | ||
* [[adi> | * [[adi> | ||
* [[adi>/ | * [[adi>/ | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
- | * [[http:// | + | |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 36: | Line 35: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-ADF4106SD1Z** evaluation board | * **EVAL-ADF4106SD1Z** evaluation board | ||
Line 42: | Line 41: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
===== Downloads ===== | ===== Downloads ===== | ||
- | | + | <WRAP round download 80%> |
+ | \\ | ||
+ | | ||
+ | * **ADF4106 Commands:** https:// | ||
+ | * **Xilinx Boards Common Drivers:** https:// | ||
+ | * **EDK KC705 Reference | ||
+ | \\ | ||
+ | </ | ||
- | The following table presents a short description the reference design archive contents. | + | ===== Hardware setup ===== |
- | ^ **Folder** ^ **Description** ^ | + | <WRAP round important 80%> |
- | | Bit | Contains | + | \\ |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore | + | Before connecting |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | </ |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe | + | |
- | ====== Run the Demonstration Project ====== | + | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. |
+ | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
- | {{page> | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-ADF4106SD1Z reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **register=** | Update the selected latch with the current set ups. Accepted value:\\ latch:\\ 0 - Reference latch\\ 1 - N Counter Latch\\ 2 - Function Latch\\ 3 - Initialization Latch\\ value:\\ 24 bit values, you can find more information about the registers in the data sheet | | ||
+ | | **register? | ||
+ | | **frequency=** | Set the VCO frequency. Accepted value:\\ 5 .. 6000 - betwwen 5Mhz and 6Ghz | | ||
+ | | **frequency? | ||
- | ===== Demonstration Project User Interface ===== | + | Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. |
- | The following | + | The following |
+ | {{ : | ||
- | {{ : | + | ===== Software Project Setup ===== |
- | + | {{page> | |
- | **Section A** allows for the communication with the board to be activated / deactivated by toggling the //ON/OFF// switch. The // | + | |
- | + | ||
- | **Sections B, C and D** allow for configuration of each latch on the **ADF4106**. | + | |
- | + | ||
- | **Section B** allows for the configuration of the //Reference Counter Latch//. The //LDP// switch allows setting the number of consecutive cycles of phase delay that must occur before Lock Detect is Set (0 = 3 Cycles, 1 = 5 Cycles). //ABP2// and //ABP1// allow setting the AntiBackLash Pulse Width. The //Slider// allows setting the R Divider. Pressing the //Write R// button programs the R Counter latch. | + | |
- | + | ||
- | **Section C** allows for the configuration of the //N Counter Latch//. The //CP Gain// switch allows toggling between different settings for the charge pump. The //B Slider// allows setting the B Counter value, while the //A Slider// allows setting the value for the A Counter. The //Write N// button programs the N Counter Latch. | + | |
- | + | ||
- | **Sections D** allows programming both the // | + | |
- | + | ||
- | ===== Troubleshooting | + | |
- | + | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | |
- | * Check that the evaluation board is powered as instructed in the board' | + | |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |