This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:fpga:xilinx:interposer:adf4001 [19 Nov 2012 18:56] – [Evaluation Boards] fix link Lars-Peter Clausen | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== ADF4001 FMC-SDP Interposer & Evaluation Board / Xilinx KC705 Reference Design ====== | ||
+ | ===== Supported Devices ===== | ||
+ | |||
+ | * [[adi> | ||
+ | |||
+ | ===== Evaluation Boards ===== | ||
+ | |||
+ | * [[adi> | ||
+ | ====== Overview ====== | ||
+ | |||
+ | This document presents the steps to setup an environment for using the **[[adi> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | For component evaluation and performance purposes, as opposed to quick prototyping, | ||
+ | * a controller board, like the **[[resources/ | ||
+ | * a compatible Analog Devices SDP [[adi> | ||
+ | * corresponding PC software | ||
+ | The **EVAL-SDP-CS1Z** controller board is Serial Interfaces Only, low cost, reduced functionality controller board. It has a USB to Serial Engine at its core. It connects to the PC through a USB 2.0 high speed port. The SDP-S has a single 120 pin connector and exposes SPI, I2C and GPIO interfaces to connected SDP daughter boards. | ||
+ | |||
+ | The **EVAL-ADF4001SD1Z** is designed to allow the user to evaluate the perfor-mance of the ADF4001 frequency synthesizer for phase-locked loops (PLLs). Figure 1 shows the board, which contains the ADF4001 synthesizer, | ||
+ | |||
+ | The ADF4001 frequency synthesizer can be used to implement clock sources for PLLs that require very low noise, stable reference signals. It consists of a low-noise digital PFD (Phase Frequency Detector), a precision charge pump, a programmable reference divider, and a programmable 13-bit N counter. In addition, the 14-bit reference counter (R Counter), allows selectable REFIN frequencies at the PFD input. A complete PLL (Phase-Locked Loop) can be implemented if the synthesizer is used with an external loop filter and VCO (Voltage Controlled Oscillator) or VCXO (Voltage Controlled Crystal Oscillator). The N min value of 1 allows flexibility in clock generation. | ||
+ | |||
+ | ===== More information ===== | ||
+ | * [[adi> | ||
+ | * [[adi>/ | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ====== Getting Started ====== | ||
+ | |||
+ | The first objective is to ensure that you have all of the items needed and to install the software tools so that you are ready to create and run the evaluation project. | ||
+ | |||
+ | ===== Required Hardware ===== | ||
+ | |||
+ | * [[http:// | ||
+ | * FMC-SDP adapter board | ||
+ | * **EVAL-ADF4001SD1Z** evaluation board | ||
+ | |||
+ | ===== Required Software ===== | ||
+ | |||
+ | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | ||
+ | * [[http:// | ||
+ | |||
+ | ===== Downloads ===== | ||
+ | |||
+ | * {{: | ||
+ | |||
+ | The following table presents a short description the reference design archive contents. | ||
+ | |||
+ | ^ **Folder** ^ **Description** ^ | ||
+ | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | ||
+ | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | ||
+ | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | ||
+ | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microblaze memory. | | ||
+ | |||
+ | ====== Run the Demonstration Project ====== | ||
+ | |||
+ | {{page> | ||
+ | |||
+ | ===== Demonstration Project User Interface ===== | ||
+ | |||
+ | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-ADF4001SD1Z** evaluation board. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | **Section A** allows for the communication with the board to be activated / deactivated by toggling the //ON/OFF// switch. The // | ||
+ | The //Error// LED will indicate that the data received on the SDO pin is different than data sent. If the //Function Latch// or // | ||
+ | |||
+ | **Sections B to E** allow for configuration of each latch on the **ADF4001**. | ||
+ | |||
+ | **Section B** allows for the configuration of the //Reference Counter Latch//. The //LDP// switch will toggle on or off the //Lock Detect Precision// bits. The //TBS// and //ABW// sliders will configure the //Test Mode Bits// and //Anti Backlash Width// bits respectively. The //14 Bit Reference Counter// allows for the configuration of the counter. The last numerical display will display the resulting value in a decimal format. By toggling the //Write// switch in this section, a single write will be performed on the //Reference Counter Latch// with the programmed value. | ||
+ | |||
+ | **Section C** allows for the configuration of the //N Counter Latch//. The //CPG// switch toggles the //CP Gain// bit. The //13 Bit N Counter// allows for the configuration of the N counter. The last numerical display in the row will display the resulting value in a decimal format. By toggling the //Write// switch, a single write will be performed on the //N Counter Latch//, with the value displayed. | ||
+ | |||
+ | **Sections D and E** have the same structure. The difference between these two latches is that when the // | ||
+ | //PD2// switch toggles the //Power Down 2// pin. The //CS2// and //CS1// sliders will configure the //Current Setting 2// and //Current Setting 1// bits respectively. The //Timer Counter Control// can be configured through the //TCC// slider. Next, the switches configure the //Fastlock Mode//, //Fastlock Enable//, //CP Three-State// | ||
+ | |||
+ | ===== Troubleshooting ===== | ||
+ | |||
+ | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | ||
+ | * Check that the evaluation board is powered as instructed in the board' | ||
+ | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | ||
+ | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | ||
+ | |||
+ | ====== More information ====== | ||
+ | {{page> |