This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad9789 [19 Jun 2012 20:59] – created rejeesh kutty | resources:fpga:xilinx:interposer:ad9789 [25 Jan 2021 19:33] – update renesas links after their web site update Robin Getz | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Introduction ===== | ===== Introduction ===== | ||
- | The [[adi>AD9739A]] is a 14-bit, | + | The [[adi>AD9789]] is a flexible four channel QAM encoder, interpolator and upconverter combined with a high performance, |
+ | |||
+ | ===== Supported Devices ===== | ||
+ | |||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | |||
+ | ===== Supported Carriers ===== | ||
+ | |||
+ | * [[xilinx> | ||
- | **HW Platform(s): | ||
- | **System:** Microblaze, AXI, UART | ||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
- | The bit file provided combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal, ADI DAC software and the programmer (IMPACT). The notes below refer to ML605, but the procedure is same for all the boards. | + | The bit file provided combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal, ADI DAC software and the programmer (IMPACT). |
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * ML605/ | + | * ML605 board |
- | * AD9739A-EBZ board & Power supply | + | * AD9789-EBZ board & Power supply |
* DAC FMC interposer board | * DAC FMC interposer board | ||
- | * Signal/ | + | * Signal/ |
* Spectrum Analyzer | * Spectrum Analyzer | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.1 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). |
* A UART terminal (Tera Term/ | * A UART terminal (Tera Term/ | ||
- | * ADI DPG DAC Software Suite [[http:// | + | * ADI DPG DAC Software Suite [[adi>en/ |
==== Bit file ==== | ==== Bit file ==== | ||
- | * Download the gzip file and extract the **sw/cf_ad9739a_ebz< | + | * Download the gzip file and extract the **sw/cf_ad9789_ebz.bit** file. |
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | |||
- | <note tip>If you are not familiar with ML605 and/or Xilix tools, please visit\\ [[http:// | ||
- | </ | ||
To begin make the following connections (see image below): | To begin make the following connections (see image below): | ||
- | * Connect the AD9739A-EBZ board to the FMC Interposer board. | + | * Connect the AD9789-EBZ board to the FMC Interposer board. |
* Connect the interposer board to the **FMC-LPC** connector of ML605 board. | * Connect the interposer board to the **FMC-LPC** connector of ML605 board. | ||
- | * Connect power to ML605 and the AD9739A-EBZ boards. | + | * Connect power to ML605 and the AD9789-EBZ boards. |
* Connect two USB cables from the PC to the //JTAG// and //UART// USB connectors on ML605. | * Connect two USB cables from the PC to the //JTAG// and //UART// USB connectors on ML605. | ||
- | * Connect a USB cable to the AD9739A-EBZ board. | + | * Connect a USB cable to the AD9789-EBZ board. |
- | * Connect an external clock source to AD9739A-EBZ board' | + | * Connect an external clock source to AD9789-EBZ board' |
- | * Connect a spectrum analyzer to AD9739A-EBZ board' | + | * Connect a spectrum analyzer to AD9789-EBZ board' |
- | Setup the clock source to be 2.5GHz. If you wish to run the device at a different clock rate, please change the SDK c program accordingly. After the hardware setup, turn the power on to the ML605 and the AD9739A-EBZ boards. | + | Setup the clock source to be 2.4GHz/6dBm. After the hardware setup, turn the power on to the ML605 and the AD9789-EBZ boards. |
- | {{: | + | {{: |
- | Start ADI- AD9739A SPI program (see screenshot below)- | + | The reference design primarily supports four modes of operation. |
- | | + | | Mode | Key-Select |
- | | + | | 0x0 | ' |
- | | + | | 0x1 | ' |
+ | | 0x2 | ' | ||
+ | | 0x3 | ' | ||
- | {{: | + | The reference design is NOT fully verified across all the modes. The delay/ |
- | Start IMPACT, and initialze the JTAG chain. The program should recognize the Virtex 6 device (see screenshot below). Start a UART terminal (set to 57600 baud rate) and then program the device. | + | ==== QAM Mapper Mode ==== |
- | {{: | + | |
+ | ==== SRRC Filter Mode ==== | ||
+ | |||
+ | |||
+ | ==== Interpolation Filter Mode ==== | ||
+ | |||
+ | Start ADI- AD9789 SPI program (see screenshot below)- | ||
+ | |||
+ | * Click on "Run Continously" | ||
+ | * Interface Control: Set DCO_INV to OFF position (change it to ON if the spectrum has unwanted spurs). | ||
+ | * Interface Control: Set I/F_MODE to Channelizer mode. | ||
+ | * Interface Control: Set CHANPRI to ON position (enabled). | ||
+ | * Data Control: Set Coding to Binary position. | ||
+ | * Data Control: Set Data Width to 16-Bit mode. | ||
+ | * Data Control: Set I/O-Data Path to Complex. | ||
+ | * Data Control: Make sure BusWidth is set to 32. | ||
+ | * Data Control: Set Latency to 1. | ||
+ | * Channel Select: Enable all channnels. | ||
+ | * Bypass: Enable QAM Mapper, SRRC filter and filter 4 bypass. | ||
+ | * Summing Junction Scalar Input Scalar: Set 2.6 Multiplier Scale to 16. Note that this value must be set so that the saturation counter is always read as 0x0. You may clear the saturation register by clicking on the knob right next to it. | ||
+ | * NCO Frequency Tuming Words: Make sure the central frequency is 834MHz on all channels. | ||
+ | * Interpolating BPF Center Frequency: Set it to 834MHz click twice on the button to the right for the changes to take effect. | ||
+ | * Reference/ | ||
+ | * Reference/ | ||
+ | * Reference/ | ||
+ | |||
+ | {{: | ||
+ | |||
+ | * Start a UART terminal (57600 baud rate). | ||
+ | * Start IMPACT/XMD then program the device. | ||
If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | ||
- | {{: | + | {{: |
- | Now enable | + | Select ' |
- | * (4) click on " | + | {{: |
- | * (5) click on " | + | |
- | * (6) make sure that " | + | |
- | After DDS is enabled, you should see the spectrum analyzer displaying the 300MHz tone. | + | ==== QDUC Mode ==== |
- | {{: | + | Start ADI- AD9789 SPI program (see screenshot below)- |
+ | |||
+ | * Click on "Run Continously" | ||
+ | * Interface Control: Set DCO_INV to OFF position (change it to ON if the spectrum has unwanted spurs). | ||
+ | * Interface Control: Set I/F_MODE to QDUC mode. | ||
+ | * Interface Control: Set CHANPRI to ON position (enabled). | ||
+ | * Data Control: Set Coding to Binary position. | ||
+ | * Data Control: Set Data Width to 16-Bit mode. | ||
+ | * Data Control: Set I/O-Data Path to Complex. | ||
+ | * Data Control: Make sure BusWidth is set to 32. | ||
+ | * Data Control: Set Latency to 1. | ||
+ | * Channel Select: Enable channel 0, disable all the other channnels. | ||
+ | * Bypass: Enable QAM Mapper, SRRC filter and all other filters bypass. | ||
+ | * Summing Junction Scalar Input Scalar: Set 2.6 Multiplier Scale to 45. Note that this value must be set so that the saturation counter is always read as 0x0. You may clear the saturation register by clicking on the knob right next to it. | ||
+ | * NCO Frequency Tuming Words: Make sure the central frequency is 834MHz on channel 0. | ||
+ | * Interpolating BPF Center Frequency: Set it to 834MHz click twice on the button to the right for the changes to take effect. | ||
+ | * Reference/ | ||
+ | * Reference/ | ||
+ | * Reference/ | ||
+ | |||
+ | {{: | ||
+ | |||
+ | * Start a UART terminal (57600 baud rate). | ||
+ | * Start IMPACT/XMD then program the device. | ||
+ | |||
+ | If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Select ' | ||
+ | |||
+ | {{: | ||
===== Using the reference design ===== | ===== Using the reference design ===== | ||
Line 79: | Line 144: | ||
==== Functional description ==== | ==== Functional description ==== | ||
- | The reference design consists of a DDS module and a lvds interface. | + | The reference design consists of a DDS module and a lvds interface. The DDS module consists of a Xilinx DDS core and DDR based DDS. It is possible to change |
- | + | ||
- | The DDS module consists of a Xilinx DDS core and DDR based DDS. Internally | + | |
==== Registers ==== | ==== Registers ==== | ||
Line 89: | Line 152: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | {{:resources: | + | FPGA Referece Designs: |
- | {{: | + | <WRAP round download 80%> |
- | {{: | + | * **ML605 (source files) ** {{: |
+ | * **ML605 (bit/sw files) ** {{: | ||
+ | </ | ||
+ | Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[/ | ||
- | ===== Notes ===== | + | <WRAP round help 80%> |
+ | * Questions? [[ez> | ||
+ | </ | ||
- | The following two files are removed from the tar file. | ||
- | * pcores/ | ||
- | * pcores/ | ||
- | To use the reference design as it is, re-generate the Xilinx DDS core for a single sine output (16bit) in full range mode. | ||
===== Tar file contents ===== | ===== Tar file contents ===== | ||
- | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http://www.xilinx.com/support/ | + | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[xilinx>support/ |
| license.txt | ADI license & copyright information. | | | license.txt | ADI license & copyright information. | | ||
Line 118: | Line 182: | ||
===== More information ===== | ===== More information ===== | ||
- | * [[http:// | + | * [[http:// |
* [[ez> | * [[ez> | ||