Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:fpga:xilinx:interposer:ad9787 [20 Feb 2012 10:47] – [Running Demo (SDK) Program] Alexandru Tofan | resources:fpga:xilinx:interposer:ad9787 [10 Feb 2021 20:16] (current) – [Introduction] - fix link Robin Getz |
---|
===== Evaluation Boards ===== | ===== Evaluation Boards ===== |
| |
* [[adi>en/digital-to-analog-converters/da-converters/ad9785/products/EVAL-AD9785/eb.html|AD9785-DPG2-EBZ]] | * [[adi>AD9785-DPG2-EBZ]] |
* [[adi>en/digital-to-analog-converters/da-converters/ad9787/products/EVAL-AD9787/eb.html|AD9787-DPG2-EBZ]] | * [[adi>AD9787-DPG2-EBZ]] |
* [[adi>en/digital-to-analog-converters/da-converters/ad9788/products/EVAL-AD9788/eb.html|AD9788-DPG2-EBZ]] | * [[adi>AD9788-DPG2-EBZ]] |
| |
===== Introduction ===== | ===== Introduction ===== |
high dynamic range TxDAC® devices, respectively, that provide a sample rate of 800 MSPS, permitting multicarrier generation up to the Nyquist frequency. Features are included for optimizing direct conversion transmit applications, including complex digital modulation, as well as gain, phase, and offset compensation. | high dynamic range TxDAC® devices, respectively, that provide a sample rate of 800 MSPS, permitting multicarrier generation up to the Nyquist frequency. Features are included for optimizing direct conversion transmit applications, including complex digital modulation, as well as gain, phase, and offset compensation. |
| |
**HW Platform(s):** [[http://www.xilinx.com/products/boards-and-kits/EK-V6-ML605-G.htm|Virtex-6 ML605 (Xilinx)]], [[adi>en/digital-to-analog-converters/da-converters/ad9785/products/EVAL-AD9785/eb.html|AD9785 Evaluation Board (ADI)]] / [[adi>en/digital-to-analog-converters/da-converters/ad9787/products/EVAL-AD9787/eb.html|AD9787 Evaluation Board (ADI)]] / [[adi>en/digital-to-analog-converters/da-converters/ad9788/products/EVAL-AD9788/eb.html|AD9788 Evaluation Board (ADI)]], [[http://www.analog.com/en/digital-to-analog-converters/da-converters/ad-dac-fmc/products/product.html|DAC FMC Interposer Board (ADI)]] \\ | **HW Platform(s):** [[xilinx>products/boards-and-kits/EK-V6-ML605-G.htm|Virtex-6 ML605 (Xilinx)]], [[adi>EVAL-AD9785|AD9785 Evaluation Board (ADI)]] / [[adi>EVAL-AD9787|AD9787 Evaluation Board (ADI)]] / [[adi>EVAL-AD9788|AD9788 Evaluation Board (ADI)]], [[adi>AD-DAC-FMC|DAC FMC Interposer Board (ADI)]] \\ |
**System:** Microblaze, AXI, UART | **System:** Microblaze, AXI, UART |
| |
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== |
| |
<note tip>If you are not familiar with ML605 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/boards/ml605/reference_designs.htm]] for details. | <WRAP tip>If you are not familiar with ML605 and/or Xilix tools, please visit\\ [[xilinx>products/boards/ml605/reference_designs.htm]] for details. |
</note> | </WRAP> |
| |
Extract the project from the archive file (AD978x.zip) to the location you desire. | Extract the project from the archive file (AD978x.zip) to the location you desire. |
- **Section 11** See datasheet pg. 32, Table 21, 22 and 23. | - **Section 11** See datasheet pg. 32, Table 21, 22 and 23. |
| |
<note important> | <WRAP important> |
* If you drag a slider and it doesn't change the value in the numeric indicator next to it, please press Stop and then Play again. At the bottom of the screen, the bytes/sec should be increasing with 200 per second. If they increase only with 50 per second, please press Stop and Play again. | * If you drag a slider and it doesn't change the value in the numeric indicator next to it, please press Stop and then Play again. At the bottom of the screen, the bytes/sec should be increasing with 200 per second. If they increase only with 50 per second, please press Stop and Play again. |
* If you receive (Pc Port Open) at the bottom of the screen, please press Stop, close your COM port, reprogram the FPGA, launch the software and try again. | * If you receive (Pc Port Open) at the bottom of the screen, please press Stop, close your COM port, reprogram the FPGA, launch the software and try again. |
</note> | </WRAP> |
===== Downloads ===== | ===== Downloads ===== |
{{:resources:fpga:xilinx:pmod:ad9116.zip|Reference design source code}} | {{:resources:fpga:xilinx:interposer:ad9787.zip|Reference design source code}} |