Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:fpga:xilinx:interposer:ad9787 [20 Feb 2012 10:47] – [Running Demo (SDK) Program] Alexandru Tofanresources:fpga:xilinx:interposer:ad9787 [10 Feb 2021 20:16] (current) – [Introduction] - fix link Robin Getz
Line 9: Line 9:
 ===== Evaluation Boards ===== ===== Evaluation Boards =====
  
-  * [[adi>en/digital-to-analog-converters/da-converters/ad9785/products/EVAL-AD9785/eb.html|AD9785-DPG2-EBZ]] +  * [[adi>AD9785-DPG2-EBZ]] 
-  * [[adi>en/digital-to-analog-converters/da-converters/ad9787/products/EVAL-AD9787/eb.html|AD9787-DPG2-EBZ]] +  * [[adi>AD9787-DPG2-EBZ]] 
-  * [[adi>en/digital-to-analog-converters/da-converters/ad9788/products/EVAL-AD9788/eb.html|AD9788-DPG2-EBZ]]+  * [[adi>AD9788-DPG2-EBZ]]
    
 ===== Introduction ===== ===== Introduction =====
Line 18: Line 18:
 high dynamic range TxDAC® devices, respectively, that provide a sample rate of 800 MSPS, permitting multicarrier generation up to the Nyquist frequency. Features are included for optimizing direct conversion transmit applications, including complex digital modulation, as well as gain, phase, and offset compensation. high dynamic range TxDAC® devices, respectively, that provide a sample rate of 800 MSPS, permitting multicarrier generation up to the Nyquist frequency. Features are included for optimizing direct conversion transmit applications, including complex digital modulation, as well as gain, phase, and offset compensation.
  
-**HW Platform(s):** [[http://www.xilinx.com/products/boards-and-kits/EK-V6-ML605-G.htm|Virtex-6 ML605 (Xilinx)]], [[adi>en/digital-to-analog-converters/da-converters/ad9785/products/EVAL-AD9785/eb.html|AD9785 Evaluation Board (ADI)]] / [[adi>en/digital-to-analog-converters/da-converters/ad9787/products/EVAL-AD9787/eb.html|AD9787 Evaluation Board (ADI)]] / [[adi>en/digital-to-analog-converters/da-converters/ad9788/products/EVAL-AD9788/eb.html|AD9788 Evaluation Board (ADI)]], [[http://www.analog.com/en/digital-to-analog-converters/da-converters/ad-dac-fmc/products/product.html|DAC FMC Interposer Board (ADI)]] \\+**HW Platform(s):** [[xilinx>products/boards-and-kits/EK-V6-ML605-G.htm|Virtex-6 ML605 (Xilinx)]], [[adi>EVAL-AD9785|AD9785 Evaluation Board (ADI)]] / [[adi>EVAL-AD9787|AD9787 Evaluation Board (ADI)]] / [[adi>EVAL-AD9788|AD9788 Evaluation Board (ADI)]], [[adi>AD-DAC-FMC|DAC FMC Interposer Board (ADI)]] \\
 **System:** Microblaze, AXI, UART **System:** Microblaze, AXI, UART
  
Line 43: Line 43:
 ==== Running Demo (SDK) Program ==== ==== Running Demo (SDK) Program ====
  
-<note tip>If you are not familiar with ML605 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/boards/ml605/reference_designs.htm]] for details. +<WRAP tip>If you are not familiar with ML605 and/or Xilix tools, please visit\\ [[xilinx>products/boards/ml605/reference_designs.htm]] for details. 
-</note>+</WRAP>
  
 Extract the project from the archive file (AD978x.zip) to the location you desire.  Extract the project from the archive file (AD978x.zip) to the location you desire. 
Line 115: Line 115:
   - **Section 11** See datasheet pg. 32, Table 21, 22 and 23.   - **Section 11** See datasheet pg. 32, Table 21, 22 and 23.
  
-<note important>+<WRAP important>
   * If you drag a slider and it doesn't change the value in the numeric indicator next to it, please press Stop and then Play again. At the bottom of the screen, the bytes/sec should be increasing with 200 per second. If they increase only with 50 per second, please press Stop and Play again.   * If you drag a slider and it doesn't change the value in the numeric indicator next to it, please press Stop and then Play again. At the bottom of the screen, the bytes/sec should be increasing with 200 per second. If they increase only with 50 per second, please press Stop and Play again.
   * If you receive (Pc Port Open) at the bottom of the screen, please press Stop, close your COM port, reprogram the FPGA, launch the software and try again.   * If you receive (Pc Port Open) at the bottom of the screen, please press Stop, close your COM port, reprogram the FPGA, launch the software and try again.
-</note>+</WRAP>
 ===== Downloads ===== ===== Downloads =====
-{{:resources:fpga:xilinx:pmod:ad9116.zip|Reference design source code}}+{{:resources:fpga:xilinx:interposer:ad9787.zip|Reference design source code}}
resources/fpga/xilinx/interposer/ad9787.txt · Last modified: 10 Feb 2021 20:16 by Robin Getz