This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad9467 [16 Jul 2015 10:51] – [Supported Carriers] Lucian Sin | resources:fpga:xilinx:interposer:ad9467 [25 Apr 2023 15:34] (current) – Modified the wrong page, so revert changes and add obsolete tag Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD9467 Evaluation Board, ADC-FMC Interposer & Xilinx Reference Design ====== | ====== AD9467 Evaluation Board, ADC-FMC Interposer & Xilinx Reference Design ====== | ||
- | + | ||
+ | <note important> | ||
===== Introduction ===== | ===== Introduction ===== | ||
Line 7: | Line 9: | ||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
- | * [[http:// | + | * [[adi>en/ |
- | * [[http:// | + | * [[adi>en/ |
===== Supported Carriers ===== | ===== Supported Carriers ===== | ||
Line 84: | Line 86: | ||
The reference design is built on a microblaze based system parameterized for linux. A functional block diagram of the design is given below. | The reference design is built on a microblaze based system parameterized for linux. A functional block diagram of the design is given below. | ||
- | {{: | + | === Xilinx block diagram === |
+ | {{: | ||
+ | |||
+ | === AD9467 FMC Card block diagram | ||
+ | {{: | ||
The reference design consists of three functional modules, a LVDS interface, a PN9/ | The reference design consists of three functional modules, a LVDS interface, a PN9/ | ||
Line 115: | Line 121: | ||
</ | </ | ||
- | Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[http:// | + | Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[/ |
<WRAP round help 80%> | <WRAP round help 80%> | ||
- | * Questions? [[http://ez.analog.com/post!input.jspa? | + | * Questions? [[ez> |
</ | </ | ||
===== Tar file contents ===== | ===== Tar file contents ===== | ||
- | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http://www.xilinx.com/support/ | + | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[xilinx>support/ |
| license.txt | ADI license & copyright information. | | | license.txt | ADI license & copyright information. | | ||
Line 134: | Line 140: | ||
- | ===== More information | + | ===== Support |
- | + | ||
- | * [[http:// | + | |
- | * [[ez> | + | |
+ | **As this design is obsolete, we do not fully support it anymore**. Analog Devices will provide **limited** online support for anyone using the reference design with Analog Devices components via the [[ez> | ||
+ | It should be noted, that the older the tools' versions and release branches are, the lower the chances to receive support from ADI engineers. |