This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad9467 [16 Jul 2015 10:51] – [Supported Carriers] Lucian Sin | resources:fpga:xilinx:interposer:ad9467 [25 Apr 2023 10:56] – Separate obsolete section Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD9467 Evaluation Board, ADC-FMC Interposer & Xilinx Reference Design ====== | ====== AD9467 Evaluation Board, ADC-FMC Interposer & Xilinx Reference Design ====== | ||
+ | This wiki page contains sections with obsolete information, | ||
+ | |||
===== Introduction ===== | ===== Introduction ===== | ||
The [[adi> | The [[adi> | ||
- | ===== Supported | + | ===== Supported |
- | * [[http:// | + | * [[adi>en/ |
- | * [[http:// | + | * [[adi>en/ |
+ | |||
+ | ===== Supported carriers ===== | ||
+ | |||
+ | * [[xilinx> | ||
+ | * [[https:// | ||
+ | * [[xilinx> | ||
+ | * [[xilinx> | ||
+ | |||
+ | ===== Quick start guide ===== | ||
+ | |||
+ | ==== Required hardware ==== | ||
+ | |||
+ | ==== Required software ==== | ||
+ | |||
+ | * ZedBoard or KC705 board | ||
+ | * AD9467-FMC-250EBZ | ||
+ | * Signal/ | ||
+ | * Signal generator (analog input, for data capture) | ||
+ | * UART terminal (Tera Term/ | ||
- | ===== Supported Carriers ===== | + | ==== Hardware modifications |
- | * [[xilinx> | + | ===== Obsolete quick start guide ===== |
- | * [[xilinx> | + | |
- | * [[xilinx> | + | |
+ | This quick start guide is kept for legacy purposes only, and the designs on carriers ML605 and VC707 are no longer supported. | ||
- | ===== Quick Start Guide ===== | + | ++++ Click to expand Obsolete |
The reference design has been tested with ML605, KC705 and VC707. The notes below refer to ML605, the procedure is same for the other boards. Please make sure you are using the correct reference design for the board(s) that you have. The bit file provided combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT). | The reference design has been tested with ML605, KC705 and VC707. The notes below refer to ML605, the procedure is same for the other boards. Please make sure you are using the correct reference design for the board(s) that you have. The bit file provided combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT). | ||
Line 23: | Line 43: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * ML605, KC705 or VC707 board | + | * ML605, KC705 or VC707 board |
* AD9467-2x0EBZ board & Power supply | * AD9467-2x0EBZ board & Power supply | ||
* ADC FMC interposer board | * ADC FMC interposer board | ||
Line 32: | Line 52: | ||
* Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | * Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | ||
- | * A UART terminal (Tera Term/ | + | * UART terminal (Tera Term/ |
==== Bit file ==== | ==== Bit file ==== | ||
Line 84: | Line 104: | ||
The reference design is built on a microblaze based system parameterized for linux. A functional block diagram of the design is given below. | The reference design is built on a microblaze based system parameterized for linux. A functional block diagram of the design is given below. | ||
- | {{: | + | === Xilinx block diagram === |
+ | {{: | ||
+ | |||
+ | === AD9467 FMC Card block diagram | ||
+ | {{: | ||
The reference design consists of three functional modules, a LVDS interface, a PN9/ | The reference design consists of three functional modules, a LVDS interface, a PN9/ | ||
Line 115: | Line 139: | ||
</ | </ | ||
- | Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[http:// | + | Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[/ |
- | <WRAP round help 80%> | ||
- | * Questions? [[http:// | ||
- | </ | ||
===== Tar file contents ===== | ===== Tar file contents ===== | ||
- | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http://www.xilinx.com/support/ | + | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[xilinx>support/ |
| license.txt | ADI license & copyright information. | | | license.txt | ADI license & copyright information. | | ||
Line 133: | Line 154: | ||
| cf_lib/ | | cf_lib/ | ||
+ | ++++ | ||
===== More information ===== | ===== More information ===== | ||
- | * [[http:// | + | * [[http:// |
* [[ez> | * [[ez> | ||
- | |||
- | |||
- |