This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad9129 [18 Oct 2012 16:52] – changed ADC to DAC Larry Welch | resources:fpga:xilinx:interposer:ad9129 [28 Jan 2021 19:13] (current) – update arrow links after their web site update Robin Getz | ||
---|---|---|---|
Line 5: | Line 5: | ||
The [[adi> | The [[adi> | ||
- | **HW Platform(s): | + | ===== Supported Devices ===== |
- | **System:** Microblaze, AXI, UART | + | |
+ | | ||
+ | * [[adi>en/ | ||
+ | |||
+ | ===== Supported Carriers ===== | ||
+ | |||
+ | | ||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
Line 24: | Line 31: | ||
* Xilinx ISE 14.1 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | * Xilinx ISE 14.1 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | ||
* A UART terminal (Tera Term/ | * A UART terminal (Tera Term/ | ||
- | * ADI DPG DAC Software Suite [[http://www.analog.com/en/ | + | * ADI DPG DAC Software Suite [[/resources/eval/dpg/dacsoftwaresuite|available here]]. |
==== Bit file ==== | ==== Bit file ==== | ||
Line 74: | Line 81: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | {{: | + | <WRAP round download 80%> |
- | + | * **ML605 Source files ** {{: | |
- | ===== Notes ===== | + | * **ML605 SW/ |
- | + | </ | |
- | The following two files are missing from the tar file. | + | |
- | * netlist/ | + | Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[/resources/eval/ |
- | * hdl/verilog/cf_ddsx.v | + | |
- | To use the reference design as it is, re-generate these two files (16bit full-range sine DDS). | + | <WRAP round help 80%> |
+ | * Questions? [[ez> | ||
+ | </ | ||
===== Tar file contents ===== | ===== Tar file contents ===== | ||
- | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http://www.xilinx.com/support/ | + | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[xilinx>support/ |
| license.txt | ADI license & copyright information. | | | license.txt | ADI license & copyright information. | | ||
Line 99: | Line 106: | ||
===== More information ===== | ===== More information ===== | ||
- | * [[http:// | + | * [[http:// |
* [[ez> | * [[ez> | ||