This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad7693 [09 Oct 2012 13:52] – created Alexandru.Tofan | resources:fpga:xilinx:interposer:ad7693 [14 Jan 2021 06:09] (current) – use xilinx> interwiki links Robin Getz | ||
---|---|---|---|
Line 29: | Line 29: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 37: | Line 37: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-AD7693SDZ** evaluation board | * **EVAL-AD7693SDZ** evaluation board | ||
Line 63: | Line 63: | ||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | <note important> | + | <WRAP important> |
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
Line 77: | Line 77: | ||
{{ : | {{ : | ||
- | <note tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' | + | <WRAP tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |