This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad7492 [04 May 2012 12:14] – created Adrian Costina | resources:fpga:xilinx:interposer:ad7492 [14 Jan 2021 06:09] (current) – use xilinx> interwiki links Robin Getz | ||
---|---|---|---|
Line 16: | Line 16: | ||
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * a compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7492SDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7492SDZ** Evaluation Board. | ||
Line 33: | Line 29: | ||
* [[adi> | * [[adi> | ||
* EVAL-AD7492SDZ evaluation board user guide is included on the CD as part of the Evaluation Board Kit | * EVAL-AD7492SDZ evaluation board user guide is included on the CD as part of the Evaluation Board Kit | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 41: | Line 37: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-AD7492SDZ** evaluation board | * **EVAL-AD7492SDZ** evaluation board | ||
Line 67: | Line 63: | ||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | <note important> | + | <WRAP important> |
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
Line 81: | Line 77: | ||
{{ : | {{ : | ||
- | <note tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' | + | <WRAP tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' |
====== More information ====== | ====== More information ====== | ||
- | * [[ez>community/ | + | {{page>ez_common}} |