This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad6673 [24 Apr 2013 11:38] – [Using the Software Reference Design] Lucian Sin | resources:fpga:xilinx:interposer:ad6673 [22 Feb 2017 19:42] – Canonical spelling of JESD204B Lars-Peter Clausen | ||
---|---|---|---|
Line 115: | Line 115: | ||
- | The reference design consists of two pcores. The JESD core consists of the GTX units and the Xilinx | + | The reference design consists of two pcores. The JESD204B |
- | The ADC interface captures and buffers data from the JESD core. The DMA interface then transfers the samples to the external DDR-DRAM. The capture is initiated by the software. The status of capture (overflow, over the range) are reported back to the software. | + | The ADC interface captures and buffers data from the JESD204B |
- | The JESD core and AD6673 core has an AXI lite interface that allows control and monitoring of the capture process. | + | The JESD204B |
Line 134: | Line 134: | ||
The Software Reference Design contains an example on how to: | The Software Reference Design contains an example on how to: | ||
* Initialize the AD6673 evaluation board | * Initialize the AD6673 evaluation board | ||
- | * Initialize the JESD HDL core | + | * Initialize the JESD204B |
* Test the ADC communication using the test patterns generated by the AD6673 | * Test the ADC communication using the test patterns generated by the AD6673 | ||
* Capture data from the AD6673 using DMA transfers | * Capture data from the AD6673 using DMA transfers |