Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:fpga:xilinx:interposer:ad6673 [22 Jul 2019 10:04] – Update no-OS driver link Andrei Drimbareanresources:fpga:xilinx:interposer:ad6673 [25 Jan 2021 19:33] (current) – update renesas links after their web site update Robin Getz
Line 7: Line 7:
 ===== Supported Devices ===== ===== Supported Devices =====
  
-  * [[http://www.analog.com/en/analog-to-digital-converters/ad-converters/ad6673/products/EVAL-AD6673/eb.html|AD6673 Evaluation Board]] +  * [[adi>EVAL-AD6673|AD6673 Evaluation Board]] 
-  * [[http://www.analog.com/en/evaluation/EVAL-ADC-FMC-INT/eb.html|ADC FMC Interposer Board]]+  * [[adi>EVAL-ADC-FMC-INT|ADC FMC Interposer Board]]
  
 {{:resources:fpga:xilinx:fmc:ad6673_ebz:ad6673-ebz.jpg|AD6673}} {{:resources:fpga:xilinx:fmc:ad6673_ebz:ad6673-ebz.jpg|AD6673}}
Line 200: Line 200:
 \\ \\
 <WRAP round important 80%> <WRAP round important 80%>
-Only Xilinx coregen xco files are provided with the HDL Reference Design. You must regenerate the IP core files using this file. See [[http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms1-ebz/reference_hdl|generating Xilinx netlist/verilog files from xco files]] for details.\\+Only Xilinx coregen xco files are provided with the HDL Reference Design. You must regenerate the IP core files using this file. See [[/resources/eval/user-guides/ad-fmcomms1-ebz/reference_hdl|generating Xilinx netlist/verilog files from xco files]] for details.\\
 \\ \\
 The software project contains 2 components: the AD6673-EBZ reference design files and the AD6673 driver. All the components have to be downloaded from the links below. The software project contains 2 components: the AD6673-EBZ reference design files and the AD6673 driver. All the components have to be downloaded from the links below.
Line 231: Line 231:
 <WRAP round help 80%> <WRAP round help 80%>
 \\ \\
-  * Questions? [[http://ez.analog.com/post!input.jspa?containerType=14&container=2061|Ask Help & Support]].+  * Questions? [[ez>fpga|Ask Help & Support]].
 \\ \\
 </WRAP> </WRAP>
resources/fpga/xilinx/interposer/ad6673.txt · Last modified: 25 Jan 2021 19:33 by Robin Getz