This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad5686r [23 Jul 2012 21:27] – Approved Andrei Cozma | resources:fpga:xilinx:interposer:ad5686r [01 Oct 2013 10:47] – changed source code (without Micrium uC-Probe), added Software Setup, remove programming with Impact Lucian Sin | ||
---|---|---|---|
Line 12: | Line 12: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * a compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5686RSDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5686RSDZ** Evaluation Board. | ||
Line 35: | Line 31: | ||
===== More information ===== | ===== More information ===== | ||
* [[adi> | * [[adi> | ||
- | * EVAL-AD5686RSDZ evaluation board user guide included on EVAL BOARD CD | + | * [[adi>/ |
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 51: | Line 46: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
+ | * The EVAL-AD5686R reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
+ | <WRAP round download 80%> | ||
+ | \\ | ||
+ | * **AD5686R Driver:** https:// | ||
+ | * **AD5686R Commands:** https:// | ||
+ | * **Xilinx Boards Common Drivers:** https:// | ||
+ | * **EDK KC705 Reference project:** https:// | ||
+ | \\ | ||
+ | </ | ||
+ | ====== Run the Demonstration Project ====== | ||
- | * {{: | + | ===== Hardware setup ===== |
- | The following table presents a short description | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting | ||
+ | </ | ||
- | ^ **Folder** ^ **Description** ^ | + | |
- | | Bit | Contains | + | * Connect |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | |
- | | uCProbeInterface | Contains | + | |
- | + | ||
- | ====== Run the Demonstration Project ====== | + | |
- | {{page>ucprobe_common}} | + | <WRAP round important 80%> |
+ | \\ | ||
+ | To power on the EVAL-AD5686R evaluation board, you need to apply +6V supply voltage to J3 connector of the board. | ||
+ | </WRAP> | ||
- | ===== Demonstration | + | ===== Reference |
+ | The following commands were implemented in this version of EVAL-AD5686R reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **reset!** | Activate a power-on reset. | | ||
+ | | **load=** | Loads selected DAC input register with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 65535 - value to be written in register. | | ||
+ | | **update=** | Update the selected DAC channel with the input register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels. | | ||
+ | | **loadAndUpdate=** | Loads and updates the selected DAC with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 65535 - value to be written in register. | | ||
+ | | **readback=** | Read back the selected DAC channels value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D. | | ||
+ | | **pwrMode=** | Set up the Power Mode of a selected channel. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ power mode:\\ 0 - normal operation.\\ 1 - 1KOhm to GND.\\ 2 - 100KOhms to GND.\\ 3 - three-state. | | ||
+ | | **pwrMode? | ||
+ | | **ldacMask=** | Set up the LDAC mask register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ set/reset mask:\\ 0 - reset LDAC mask for the selected channel.\\ 1 - set LDAC mask for the selected channel. | | ||
+ | | **ldacMask? | ||
+ | | **intRef=** | Turns on or off the internal reference. Accepted values:\\ 0 - turns off the internal reference.(default)\\ 1 - turns on the internal reference. | | ||
+ | | **intRef?** | Displays the status of the internal reference. | | ||
+ | | **ldacPin=** | Sets the output value of LDAC pin. Accepted values:\\ 0 - sets LDAC pin low.(default)\\ 1 - sets LDAC pin high. | | ||
+ | | **ldacPin? | ||
- | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5686r** evaluation board. | ||
- | {{ : | + | Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. |
- | The communication with the board is activated / deactivated by toggling the **// | + | The following image shows a generic list of commands in a serial terminal connected |
+ | {{ : | ||
- | ===== Troubleshooting | + | ===== Software Project Setup ===== |
+ | {{page> | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | ||
- | * Check that the evaluation board is powered as instructed in the board' | ||
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | ||
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | ||
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |