This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad5684r [28 Sep 2012 11:21] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costina | resources:fpga:xilinx:interposer:ad5684r [01 Oct 2013 11:13] – changed source code (without Micrium uC-Probe), added Software Setup, remove programming with Impact Lucian Sin | ||
---|---|---|---|
Line 12: | Line 12: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
Line 33: | Line 33: | ||
* EVAL-AD5684RSDZ evaluation board user guide included on EVAL BOARD CD | * EVAL-AD5684RSDZ evaluation board user guide included on EVAL BOARD CD | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 47: | Line 46: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
+ | * The EVAL-AD5684R reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
+ | <WRAP round download 80%> | ||
+ | \\ | ||
+ | * **AD5684R Driver:** https:// | ||
+ | * **AD5684R Commands:** https:// | ||
+ | * **Xilinx Boards Common Drivers:** https:// | ||
+ | * **EDK KC705 Reference project:** https:// | ||
+ | \\ | ||
+ | </ | ||
+ | ====== Run the Demonstration Project ====== | ||
- | * {{: | + | ===== Hardware setup ===== |
- | The following table presents a short description the reference design archive contents. | + | <WRAP round important 80%> |
- | + | \\ | |
- | ^ **Folder** ^ **Description** ^ | + | Before connecting |
- | | Bit | Contains | + | </ |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore | + | |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe | + | |
- | + | ||
- | ====== Run the Demonstration Project ====== | + | |
- | {{page> | + | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. |
+ | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
- | ===== Demonstration Project User Interface ===== | + | <WRAP round important 80%> |
+ | \\ | ||
+ | To power on the EVAL-AD5684R evaluation board, you need to apply +6V supply voltage to J3 connector of the board. | ||
+ | </ | ||
- | The following | + | ===== Reference Project Overview ===== |
+ | The following | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **reset!** | Activate a power-on reset. | | ||
+ | | **load=** | Loads selected DAC input register with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 4095 - value to be written in register. | | ||
+ | | **update=** | Update the selected DAC channel with the input register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels. | | ||
+ | | **loadAndUpdate=** | Loads and updates | ||
+ | | **readback=** | Read back the selected DAC channels value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D. | | ||
+ | | **pwrMode=** | Set up the Power Mode of a selected channel. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ power mode:\\ 0 - normal | ||
+ | | **pwrMode? | ||
+ | | **ldacMask=** | Set up the LDAC mask register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ set/reset mask:\\ 0 - reset LDAC mask for the selected channel.\\ 1 - set LDAC mask for the selected channel. | | ||
+ | | **ldacMask? | ||
+ | | **intRef=** | Turns ON or OFF the internal reference. Accepted values:\\ 0 - turns OFF the internal reference.(default)\\ 1 - turns ON the internal reference. | | ||
+ | | **intRef?** | Displays the status | ||
+ | | **ldacPin=** | Sets the output value of LDAC pin. Accepted values:\\ 0 - sets LDAC pin low.(default)\\ 1 - sets LDAC pin high. | | ||
+ | | **ldacPin?** | Displays the value of LDAC pin. | | ||
- | {{ : | ||
- | The communication with the board is activated / deactivated by toggling the **// | + | Commands can be executed using a serial terminal connected |
- | ===== Troubleshooting ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ : | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | ===== Software Project Setup ===== |
- | * Check that the evaluation board is powered as instructed in the board' | + | {{page> |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |