This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad5542a [28 Sep 2012 11:14] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costina | resources:fpga:xilinx:interposer:ad5542a [11 Sep 2013 10:52] – changed source code (without using Micrium uC-Probe), added Sofware Setup, remove programming with Impact Lucian Sin | ||
---|---|---|---|
Line 12: | Line 12: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
Line 30: | Line 30: | ||
* {{: | * {{: | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 44: | Line 43: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
+ | * The EVAL-AD5542A reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
+ | <WRAP round download 80%> | ||
+ | \\ | ||
+ | * {{: | ||
+ | * **AD5542A Driver:** https:// | ||
+ | * **AD5542A Commands:** https:// | ||
+ | * **Xilinx Boards Common Drivers:** https:// | ||
+ | * **EDK KC705 Reference project:** https:// | ||
+ | \\ | ||
+ | </ | ||
- | * {{: | ||
- | The following table presents a short description the reference design archive contents. | + | ===== Hardware setup ===== |
- | ^ **Folder** ^ **Description** ^ | + | <WRAP round important 80%> |
- | | Bit | Contains | + | \\ |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore | + | Before connecting |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | </ |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe | + | |
- | ====== Run the Demonstration Project ====== | + | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. |
+ | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
- | {{page>ucprobe_common}} | + | <WRAP round important 80%> |
+ | \\ | ||
+ | To power on the EVAL-AD5542A evaluation board, you need to provide external +5V and -5V supply voltage. | ||
+ | </WRAP> | ||
- | ===== Demonstration Project User Interface | + | ===== Quick start evaluation |
+ | For a quick start evaluation, run the **download.bat** script located in the **SDK/ | ||
- | The following figure presents the **uC-Probe** interface | + | <WRAP round info 80%> |
+ | \\ | ||
+ | The **download.bat** script assumes | ||
+ | </ | ||
- | {{ : | + | If programming was successful, you should be seeing the command messages appear on the terminal. |
- | * The communication with the board is activated / deactivated by toggling the **//ON/OFF//** switch. The **// | + | ===== Reference Project Overview ===== |
- | * The **//DAC//** switch is used to enable/ | + | The following commands were implemented in this version of EVAL-AD5542A reference project for Xilinx KC705 FPGA board. |
- | * The **//LDAC//** switch is used to control | + | ^ Command ^ Description ^ |
- | * The **//CLR//** switch is used to control | + | | **help?** | Displays all available commands. | |
- | * The **//DAC Value//** slider is used to set the value to be loaded into the DAC register. The selected value is displayed in the numeric box next to the slider. | + | | **register=** | Writes to the DAC register. Accepted values:\\ 0 .. 65535 - |
+ | | **register?** | Displays last written value in the DAC register. | | ||
+ | | **voltage=** | Sets the DAC output voltage. Accepted values:\\ -2500 .. +2500 - desired output voltage in milivolts. | | ||
+ | | **voltage?** | Displays last written voltage value to the DAC. | | ||
+ | | **ldacPin=** | Sets the output value of LDAC pin. Accepted values:\\ 0 - sets LDAC pin low.(default)\\ 1 - sets LDAC pin high. | | ||
+ | | **ldacPin?** | Displays | ||
+ | | **clrPin=** | Sets the output value of CLR pin. Accepted values:\\ 0 - sets CLR pin low.\\ 1 - sets CLR pin high.(default) | | ||
+ | | **clrPin?** | Displays | ||
- | ===== Troubleshooting ===== | ||
- | In case there is a communication problem with the board the follwing actions | + | Commands |
- | * Check that the evaluation board is powered as instructed | + | |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols//**. | + | The following image shows a generic list of commands |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | {{ : |
+ | |||
+ | |||
+ | ===== Software Project Setup ===== | ||
+ | {{page> | ||
====== More information ====== | ====== More information ====== | ||
* [[resources: | * [[resources: | ||
{{page> | {{page> |