This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad5252 [28 Sep 2012 11:29] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costina | resources:fpga:xilinx:interposer:ad5252 [16 Oct 2013 15:05] – Delete ucProbe references, added UART interfaces snapshot, description Istvan Csomortani | ||
---|---|---|---|
Line 11: | Line 11: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
Line 29: | Line 29: | ||
* [[adi>/ | * [[adi>/ | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 43: | Line 42: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
===== Downloads ===== | ===== Downloads ===== | ||
+ | <WRAP round download 80%> | ||
+ | \\ | ||
+ | * **AD5252 Driver:** https:// | ||
+ | * **AD5252 Commands:** https:// | ||
+ | * **Xilinx Boards Common Drivers:** https:// | ||
+ | * **EDK KC705 Reference project:** https:// | ||
+ | \\ | ||
+ | </ | ||
- | * {{: | + | ===== Hardware setup ===== |
+ | <WRAP round important 80%> | ||
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. | ||
+ | </ | ||
- | The following table presents a short description | + | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. |
+ | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
- | ^ **Folder** ^ **Description** ^ | + | ===== Reference Project Overview ===== |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | | + | |
- | ====== Run the Demonstration Project | + | The following commands were implemented in this version of EVAL-AD5252 reference project for Xilinx KC705 FPGA board. |
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **rdac=** | Load the wiper register with a give value. Accepted values:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register.\\ value:\\ 0 .. 255 - value to be written in register. | | ||
+ | | **rdac?** | Read back the value of the wiper register. Accepted values:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **reset!** | Reset all wiper register to its stored values | | ||
+ | | **restore=** | Restore the specified wiper register setting form the memory. Accepted value:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **save=** | Save the given wiper register settings to the memory. Accepted value:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **writemem=** | Write to one of the user memory address. Accepted value:\\ address: a value between 0x2 and 0xE.\\ data: a value between 0 and 255.| | ||
+ | | **readmem=** | Read data from the EEMEM memory. Accepted value: | ||
+ | | **decrdacdb=** | Decrement a given wiper register by 6dB. Accepted value:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **decrdacdball!** | Decrement all wiper register by 6dB. | | ||
+ | | **decrdac=** | Decrement a given wiper register by one. Accepted value:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **decrdacall!** | Decrement all wiper register by one. | | ||
+ | | **incrdacdb=** | Increment a given wiper register by 6dB. Accepted value:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **incrdacdball!** | Increment all wiper register by 6dB. | | ||
+ | | **incrdac=** | Increment a given wiper register by one. Accepted value:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **incrdacall!** | Increment all wiper register by one. | | ||
+ | | **setwp=** | Set the state of the Write Protect (WP) pin. Accepted value:\\ desired state:\\ 0 - inactive\\ 1 - active | | ||
+ | | **getwp?** | Return the current value of the Write Protect (WP) pin | | ||
+ | | **sethwreset=** | Set the state of the Hardware Override Preset (PR) pin. Accepted value:\\ 0 - inactive\\ 1 - active | | ||
+ | | **gethwreset? | ||
+ | | **tolerance=** | Read one of the Tolerance register. Accepted value:\\ 0x0 .. 0x3 - virtual address of the tolerance register | | ||
- | {{page> | + | Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. |
- | ===== Demonstration Project User Interface ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ : | ||
- | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5252SDZ** evaluation board. | + | ===== Software Project Setup ===== |
+ | {{page> | ||
- | {{ : | ||
- | |||
- | **Section A** is used to activate the board and monitor activity. The communication with the board is activated / deactivated by toggling the **// | ||
- | |||
- | **Section B** is used to update the RDAC registers. The RDAC registers can be updated by selecting a desirable value on the slider and clicking **//Load RDACx//**. | ||
- | |||
- | **Section C** is used to read/write data from/into memory block. The location can be chosen from the EEMEM slider. Each location can be read, or updated with the value from the second slider. | ||
- | |||
- | **Section D** is used to display the stored tolerance of each internal resistor. | ||
- | |||
- | **Section E** is used to send two bytes to the AD5252 circuit. A customized I2C data-word can be sent by manually switching the buttons from 0 to 1 or from 1 to 0 as desired and then clicking **//Send Data//**. | ||
- | |||
- | **Section F** is used to enable or disable the AD5252 WP pin. | ||
- | |||
- | **Section G** is used to send the AD5252 quick commands directly to the AD5252. | ||
- | |||
- | |||
- | ===== Troubleshooting ===== | ||
- | |||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | ||
- | * Check that the evaluation board is powered as instructed in the board' | ||
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | ||
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | ||
====== More information ====== | ====== More information ====== | ||
* [[resources: | * [[resources: | ||
{{page> | {{page> |