This is an old revision of the document!
This document presents the steps to setup an environment for using the EVAL-AD5111SDZ evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). Below is presented a picture of the EVAL-AD5111SDZ Evaluation Board with the Xilinx KC705 board.
For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to use the part evaluation setup. This consists of:
The SDP-B controller board is part of Analog Devices System Demonstration Platform (SDP). It provides a high speed USB 2.0 connection from the PC to the component evaluation board. The PC runs the evaluation software. Each evaluation board, which is an SDP compatible daughter board, includes the necessary installation file required for performance testing.
Note: it is expected that the analog performance on the two platforms may differ.
Below is presented a picture of SDP-B Controller Board with the EVAL-AD5111SDZ Evaluation Board.
The EVAL-AD5111SDZ evaluation board is a member of a growing number of boards available for the SDP. Designed to help customers evaluate performance or quickly prototype new AD5111 circuits and reduce design time, the EVAL-AD5111SDZ evaluation board can operate in single-supply and incorporates an internal power supply powered from the USB.
The AD5111 provides a nonvolatile solution for 128-/64-/32-position adjustment applications, offering guaranteed low resistor tolerance errors of ±8% and up to ±6 mA current density in the A, B, and W pins. The low resistor tolerance, low nominal temperature coefficient, and high bandwidth simplify open-loop applications, as well as tolerance matching applications. The new low wiper resistance feature minimizes the wiper resistance in the extremes of the resistor array to only 45 Ω, typical. A simple 3-wire up/down interface allows manual switching or high speed digital control with clock rates up to 50 MHz.
The first objective is to ensure that you have all of the items needed and to install the software tools so that you are ready to create and run the evaluation project.
Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.
The following commands were implemented in this version of EVAL-AD5111 reference project for Xilinx KC705 FPGA board.
Command | Description |
---|---|
help? | Displays all available commands. |
increment= | Increases the resistor value with a number of steps. Accepted values: 0 .. 128 - number of steps to increment RDAC value. |
decrement= | Decreases the resistor value with a number of steps. Accepted values: 0 .. 128 - number of steps to decrement RDAC value. |
store! | Device memorizes the current RDAC value in EEPROM. |
shutdown! | Device enters in shutdown mode. |
Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA.
The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral.
The hardware platform for each reference projects with FMC-SDP interposer and KC705 evaluation board is common. The next steps should be followed to recreate the software project of the reference design: