This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad5111 [16 Mar 2012 12:07] – [Demonstration Project User Interface] Alexandru Tofan | resources:fpga:xilinx:interposer:ad5111 [09 Jan 2021 00:39] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 4: | Line 4: | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
Line 11: | Line 12: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * a compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5111SDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5111SDZ** Evaluation Board. | ||
Line 35: | Line 32: | ||
* [[adi> | * [[adi> | ||
* [[adi>/ | * [[adi>/ | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
- | * [[http:// | + | |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 44: | Line 40: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-AD5111** evaluation board | * **EVAL-AD5111** evaluation board | ||
Line 50: | Line 46: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
+ | * The EVAL-AD5111 reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | + | <WRAP round download 80%> | |
- | * {{:resources: | + | \\ |
- | + | * **AD5111 Driver:** https://github.com/ | |
- | The following table presents a short description the reference design archive contents. | + | * **AD5111 Commands:** https:// |
- | + | | |
- | ^ **Folder** ^ **Description** ^ | + | * **EDK KC705 Reference |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | \\ |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | </ |
- | | Software | Contains the source files of the software | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | | + | |
====== Run the Demonstration Project ====== | ====== Run the Demonstration Project ====== | ||
- | {{page> | + | ===== Hardware setup ===== |
- | + | ||
- | ===== Demonstration Project User Interface | + | |
- | + | ||
- | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5111SDZ** evaluation board. | + | |
- | {{ : | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. | ||
+ | </ | ||
- | **Section A** is used to activate | + | |
+ | | ||
- | **Section B** is used to set the operation | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-AD5111 reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **increment=** | Increases the resistor value with a number of steps. Accepted values:\\ 0 .. 128 - number of steps to increment RDAC value. | | ||
+ | | **decrement=** | Decreases | ||
+ | | **store!** | Device memorizes the current RDAC value in EEPROM. | | ||
+ | | **shutdown!** | Device enters in shutdown | ||
- | **Section C** is used to set the value programmed in high speed mode, using the slider provided. | ||
- | **Section D** is used to simulate a buton. By clicking it, you can increase/ | + | Commands can be executed using a serial terminal connected |
- | **Section E** displays the current position | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
- | ===== Troubleshooting ===== | + | {{ : |
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | ===== Software Project Setup ===== |
- | * Check that the evaluation board is powered as instructed in the board' | + | {{page> |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
- | * [[ez>community/ | + | {{page>ez_common}} |